Skip to main content
AHsu.1
Associate
Feb 8, 2021 8:20 AM UTC
Question

How to reset/restart mcu after DFU programming?

Hi there,

Use DfuSe v3.0.6, upgrade success and click "Leave DFU mode"

but mcu can't be reset/start?

Thanks

This topic has been closed for replies.

2 replies

Uwe Bonnes
Chief
Feb 9, 2021 9:30 AM UTC

with dfu-utils I do "dfu-util -s 0x08000000:leave -D <file.bin>"

PVasq.1
Visitor II
May 5, 2021 1:40 PM UTC

Hello AHsu.1 I have the same problem here. Did you find something on this subject?

Thank you Uwe,

For the windows users is there any solution?

Is there an specific function in DfuSE source code to perform the disconnection function?

I'm using a STM32F072 and running virtual UART through the USB port.

I'm wondering if it is possible to get access to the shell via virtual UART without the need of disconnecting and reconnecting the cable.

Thanks!