Skip to main content
Senior
Aug 6, 2024 5:58 PM UTC
Question

How to Reset an UART after an error

Hi,

Recently, we desighed a test board with STM32F103RB for UART communication with a wireless chip, and we found that the HAL_UART_ErrorCallback is triggered occasionally (the periods of errors vary betweent tens of minutes to hundreds of minutes), the error does not affect sending data from STM32F103RB to the wireless chip, but once an error occurs, the MCU does not receive any data from the wireless chip any more, at the moment, we have to reset the MCU to resolve this issue. However, we would like to reset the UART to resolve the issue if possible as there are some other tasks running on the MCU.

We tried the following, but it does not work:

HAL_UART_Abort_IT(uart);

HAL_UART_DeInit(uart);

uart->Instance = USART3;

uart->Init.BaudRate = WirelessUartBaudRate;

uart->Init.WordLength = UART_WORDLENGTH_8B;

uart->Init.StopBits = UART_STOPBITS_1;

uart->Init.Parity = UART_PARITY_NONE;

uart->Init.Mode = UART_MODE_TX_RX;

uart->Init.HwFlowCtl = UART_HWCONTROL_NONE;

uart->Init.OverSampling = UART_OVERSAMPLING_16;

HAL_UART_Init(uart);

 

What is the correct way to do this?

Many thanks to any suggestion.

Chao

 

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
Aug 6, 2024 6:16 PM UTC

Normally you'd check the status and then explicitly or implicitly clear the error conditions.

On the F1's many of the receive error can be cleared by reading the DR,

ie

if (USART3->SR & Errors) // Noise, Framing, Parity, etc

 USART3->DR;

Would suggest browsing the Reference Manual, USART register sections.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Karl Yamashita
Super User
Aug 7, 2024 12:25 AM UTC

If the UART doesn't interrupt after awhile, then the interrupt wasn't successfully enabled. This happens if you don't check the HAL return status to be sure it returned HAL_OK

 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
ST Technical Moderator
Aug 7, 2024 9:03 AM UTC

Hello @Chao 

 

In your UART reset process you are not checking if the abort, Init and DeInit are successfully done. To do this please use the function below. 

void Reset_UART(UART_HandleTypeDef *huart) {

 // Clear any pending error flags
 __HAL_UART_CLEAR_FLAG(huart, UART_CLEAR_PEF | UART_CLEAR_FEF | UART_CLEAR_NEF | UART_CLEAR_OREF);

 // Abort ongoing UART transfer
 if (HAL_UART_Abort_IT(huart) != HAL_OK) {
 // Abort Error
 Error_Handler();
 }

 // Deinitialize the UART
 if (HAL_UART_DeInit(huart) != HAL_OK) {
 // Deinitialization Error
 Error_Handler();
 }

 // Reinitialize the UART
 huart->Instance = USART3;
 huart->Init.BaudRate = WirelessUartBaudRate;
 huart->Init.WordLength = UART_WORDLENGTH_8B;
 huart->Init.StopBits = UART_STOPBITS_1;
 huart->Init.Parity = UART_PARITY_NONE;
 huart->Init.Mode = UART_MODE_TX_RX;
 huart->Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart->Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(huart) != HAL_OK) {
 // Initialization Error
 Error_Handler();
 }
}

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
ChaoAuthor
Senior
Sep 3, 2024 3:15 PM UTC

Hi  @Saket_Om 

I did checks on the returns as you suggested :

 

 

void Uart::Reset()
{

 // Clear any pending error flags
 __HAL_UART_CLEAR_FLAG(uart, UART_FLAG_CTS | UART_FLAG_LBD | UART_FLAG_TC | UART_FLAG_RXNE);
 // 这将同时清除 PE FE NE ORE 等4个FLAG
 __HAL_UART_CLEAR_PEFLAG(uart);

 // Abort ongoing UART transfer
 if (HAL_UART_Abort_IT(uart) != HAL_OK) {
 // Abort Error
 	resetError = 1;
 }

 // Deinitialize the UART
 if (HAL_UART_DeInit(uart) != HAL_OK) {
 // Deinitialization Error
 	resetError = 0x2;
 }

 // Reinitialize the UART
 uart->Instance = USART3;
 uart->Init.BaudRate = WirelessUartBaudRate;
 uart->Init.WordLength = UART_WORDLENGTH_8B;
 uart->Init.StopBits = UART_STOPBITS_1;
 uart->Init.Parity = UART_PARITY_NONE;
 uart->Init.Mode = UART_MODE_TX_RX;
 uart->Init.HwFlowCtl = UART_HWCONTROL_NONE;
 uart->Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(uart) != HAL_OK) {
 // Initialization Error
 	resetError = 0x4;
 }
}

and retrieved resetError, and found resetError=0 that means all are HAL_OK.

However, it still sometimes works and some other times does not work as before.