Skip to main content
radeshsharma
Associate II
Aug 14, 2022 9:18 PM UTC
Question

How to Record audio in STM32U5 (B-U585I-IOT02A)

Hello Community,

I'm working on stm32u5(B-U585I-IOT02A). B-U585I-IOT02A has two digital mics, and St officially has an example of BSP to record audio.

So after taking references from: https://github.com/STMicroelectronics/STM32CubeU5/blob/main/Projects/B-U585I-IOT02A/Examples/BSP/Src/audio_record.c

I've started the project but I'm getting issues with initializing BSP_AUDIO_IN_Init(0, &AudioInit), when I'm calling this function I'm getting: bsp_error_periph_failure(-4)

I don't know where I'm lagging can anyone provide me a solution to fix this error?

I really appreciate any help you can provide.

This topic has been closed for replies.

2 replies

ST Employee
Aug 16, 2022 8:36 AM UTC

Hi @radeshsharma​ ,

Can you check that you are using the right microphone (AUDIO_IN_DEVICE_DIGITAL 1 OR 2)? And that it is connected to the right place?

Regards,

DianeP

radeshsharma
Associate II
Aug 26, 2022 7:48 PM UTC

Hello @Diane POMABIA​ 

Thanks for your response. I was using AUDIO_IN_DEVICE_DIGITAL_MIC1 it was throwing bsp_error_periph_failure(-4), but after changing it to AUDIO_IN_DEVICE_DIGITAL_MIC2 it didn't throw any error but still, the recording didn't start. I tried to debug it. So, I tried to run the code line by line and I got to know things were becoming no response after reaching inside int32_t BSP_AUDIO_IN_Record(uint32_t Instance, uint8_t *pData, uint32_t NbrOfBytes)--> HAL_MDF_AcqStart_DMA(&haudio_in_mdf_filter[1], &filterConfig, &dmaConfig) --> MDF_AcqStart(hmdf, pFilterConfig); at this point code doesn't response anything, didn't throw any error just go loop.

Do you have any suggestions on this?