Skip to main content
Antek
Associate
January 8, 2021
Solved

How to properly import project to CubeIDE from xCubeAudio examples?

  • January 8, 2021
  • 6 replies
  • 2075 views

Hi, I am trying to do some audio project based on STM32F7/F4 series. I have got STM32F769I-DISCO board. I have downloaded x-cube-audio v.1.1.1 and x-cube-usb-audio v.1.0.0.

I have unpacked both packages and I am trying to build and run some example (starting from Import->Existing project into workspace). Every project that I am trying to build ends up with "Nothing to build for project..." in CubeIDE. What is the best way to start with such examples?

This topic has been closed for replies.
Best answer by Peter BENSCH

Maybe you have been a bit confused while trying to import.

In older projects like this one you can find some project files for different target GUI. In this case there is:

  • EWARM (IAR)
  • MDK-ARM (Keil)
  • SW4STM32 (AC6)

The latter one can directly be imported into STM32CubeIDE using

  • File > Import...
  • Select General > Import ac6 System Workbench for STM32 Project
  • Insert the path to the project (e.g. C:\[xyz]\Projects\STM32746G-Discovery\Applications\Audio\Audio_BAM) into the field Import source
  • Make sure to only select the line where Import as is set to Eclipse project
  • Click finish

Good luck!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

6 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
January 8, 2021

Maybe you have been a bit confused while trying to import.

In older projects like this one you can find some project files for different target GUI. In this case there is:

  • EWARM (IAR)
  • MDK-ARM (Keil)
  • SW4STM32 (AC6)

The latter one can directly be imported into STM32CubeIDE using

  • File > Import...
  • Select General > Import ac6 System Workbench for STM32 Project
  • Insert the path to the project (e.g. C:\[xyz]\Projects\STM32746G-Discovery\Applications\Audio\Audio_BAM) into the field Import source
  • Make sure to only select the line where Import as is set to Eclipse project
  • Click finish

Good luck!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Antek
AntekAuthor
Associate
January 11, 2021

I am not sure what I was doing wrong but something is starting to work.

Still I warn everyone that paths are really long with these libraries.

I attach screen with correct import.0693W000006IANtQAO.bmp

Antek
AntekAuthor
Associate
January 8, 2021

Thanks for this nice explanation. I have tried what You wrote. Problem was probably also with very long path. After shortening I was able to find this Eclipse project.

Despite this fact, I am still struggling to build, now I have no configuration to choose, do I need to set it manually?

0693W000006I0nSQAS.bmp

Cartu38 OpenDev
Graduate II
January 8, 2021

@Antek​  Try to remove imported materiel and redo promoting full path (....../SW4STM32/MP3-STM32F746G-DISCO) ... sounds to me you've not initiated import from proper level. Obviously you should have build configuration set for you if import done properly.

Antek
AntekAuthor
Associate
January 11, 2021

Did anyone try to do that with audio libraries and newest CubeIDE? I am still struggling.

GOtté.1
Visitor II
January 12, 2021

Me too. What a shame. such a beautiful hardware, but what a messy software :sleepy_face: