Skip to main content
Luc T
Associate II
May 8, 2019
Question

How to program a STM32 Nucleo board via Ethernet interface?

  • May 8, 2019
  • 0 replies
  • 534 views

Hi,

is there a way to program a STM32 Nucleo board (Nucleo-F767ZI) via the Ethernet interface?

The problem with the usb port is when the Nucleo 5V is powered externally via the E5V pin, at power on of the 5V, the usb cable must be removed. So on a remote system someone has to connect the usb cable first before I can program the Nucleo. So if I can program the Nucleo via the Ethernet interface, I can avoid this problem.

Best regards,

Luc

This topic has been closed for replies.