How to jump to the system memory bootloader of STM32L4R5 controller?
Hello,
we are using Custom board of STM32L4R5 micro-controller.
As per the boot configuration at section 2.6, we have set the nBOOT1 bit to 1, nBOOT0 set to zero, BOOT0 pin set to zero, nSWBOOT0 bit set to zero to enable and jump to the system memory bootloader.
As below,
SET_BIT(FLASH->OPTR, FLASH_OPTR_nBOOT1);
CLEAR_BIT(FLASH->OPTR, FLASH_OPTR_nBOOT0);
CLEAR_BIT(FLASH->OPTR, FLASH_OPTR_nSWBOOT0);
And tried to jump to the address 0x1FFF0000, but not able to jump.
Please provide the sequence if any required or missing any thing from my side.
Thank you.