Skip to main content
KHofm.1
Associate II
Jun 29, 2022 9:39 AM UTC
Question

How to jump to bootloader from application using STM32U585?

Hi there,

using the STM32U585 I try to jump from application into bootloader. Could somebody please share some code that I could use, instead of this piece that does not do its job?

void JumpToBootloader(void)
{
 void (*SysMemBootJump)(void);
 volatile uint32_t addr = 0x0BF90000;
	
 HAL_I2C_DeInit(&hi2c1);
 HAL_I2C_DeInit(&hi2c2);
 USBD_DeInit(&hUsbDeviceFS);
 HAL_RCC_DeInit();
 
 SysTick->CTRL = 0;
 SysTick->LOAD = 0;
 SysTick->VAL = 0;
 
 __disable_irq();
 
 SYSCFG->CFGR1 = 0x01;
 __DSB();
 
 SysMemBootJump = (void (*)(void)) (*((uint32_t *)(addr + 4)));
 
 __set_MSP(*(uint32_t *)addr);
 
 SysMemBootJump();
}

Besides: do I have to pay attention to something special, when using FreeRTOS?

Thanks in advance,

This topic has been closed for replies.

5 replies

Uwe Bonnes
Chief
Jun 29, 2022 10:51 AM UTC

Deinitialising everything may be difficult. I.m.h.o. best thing is to have a switch early in the startup code before RAM is initialized or use RAM that is not initialized. When jump to bootloader is needed, set some magic in ram and reset. When bootswitch sees the magic, it remove the magic and jumps to bootloader. When no magic is seen, eventually also check for valid code and when not found, jump to bootloader too.

KHofm.1
KHofm.1Author
Associate II
Jun 29, 2022 11:08 AM UTC

Thank you Uwe,

would you please share a link with an example?

Best,

Kai

Uwe Bonnes
Chief
Jun 29, 2022 11:29 AM UTC

https://github.com/bl*ckm*g*c-debug/bl*ckm*g*c/blob/main/src/platforms/f072/platform.c

Sorry for the obfuscation, but big brother blocks w/o obfuscation...

KHofm.1
KHofm.1Author
Associate II
Jun 29, 2022 11:38 AM UTC

tried now this:

/*...snip*/
/* Call the clock system initialization function.*/
 bl SystemInit
/* Call static constructors */
 bl __libc_init_array
 
/* check for a magic constant in RAM, if present brach to bootloader */
 LDR R0, =0x2000FFF0
 LDR R1, =0xDEADBEEF
 LDR R2, [R0, #0]
 STR R0, [R0, #0] /* Invalidate*/
 CMP R2, R1
 BEQ Reboot_Loader
 
/* Call the application's entry point.*/
	bl	main
 
LoopForever:
 b LoopForever
 
.size	Reset_Handler, .-Reset_Handler
 
Reboot_Loader:
 LDR R0, =0x0BF90000
 LDR SP,[R0, #0]
 LDR R0,[R0, #4]
 BX R0
/*...snip*/

and this:

void JumpToBootloader(void)
{
	*((unsigned long *)0x2000FFF0) = 0xDEADBEEF; 
	NVIC_SystemReset();
}

took from: 'https://www.mikrocontroller.net/articles/STM32_jump_to_bootloader'.

Debugging this, I can see the jump to 'Reboot_Loader:' after Reset and then the jump to the bootloader's section.

Using it without debugger, it even works!

Thanks for the hint, Uwe!

ST Technical Moderator
Jul 2, 2022 2:58 PM UTC

Hello @KHofm.1​ ,

This document, AN2606 STM32 microcontroller system memory boot mode, gives all the details about: How to jump in bootloader from user application.

Note that on some STM32 with flash empty check mechanism, it's not possible to jump in the bootloader from your application running in the user flash.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks