Skip to main content
Associate
August 17, 2026
Question

How to intentionally trigger a blocking failure on STM32N6570-DK to test PG10 BootFailed output

Hello,

I am trying to intentionally force a blocking failure on the STM32N6570-DK to observe how the system handles the error and to test the PG10 BootFailed UART output.

To do this, I have tried tampering with the FSBL header in various ways to force a failure, as well as simply erasing the OctaFlash.

However, despite my attempts, no ID code or valid UART output ever arrives on PG10.

While the Boot ROM manual (UM3234) describes what happens during a blocking failure, there are no clear notes or official procedures explaining how a blocking failure can be intentionally generated for testing purposes.

Could someone from ST or the community clarify:

How can we intentionally and reliably trigger a blocking failure on the STM32N6570-DK to test the PG10 BootFailed UART output?

Any guidance or suggestions would be greatly appreciated.

Best regards

2 replies

ST Technical Moderator
August 18, 2026

Hello ​@Jimmy7 

If we take serial boot as an example, we should try using a USB cable to perform a download and then unplug the USB cable in the middle of the download. That should cause a blocking failure.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Associate II
August 19, 2026

Please refer the document below for help

Handling of soft errors in STM32 applications