Skip to main content
Associate
Dec 20, 2024 2:04 PM UTC
Solved

How to integrate netXDuo azure_iot addon with third-party device

Hi,

The requirement is to port MQTT of NetX Duo to STM32f412 ,without the need to use the TCP/IP and TLS addons in NetX Duo.  Since we have DIGI XBee's modem and we will use its  TLS socket for communications. I have the secure-socket-like interface ready, e.g. createSocket, connect, send, recv, etc...I'm looking at the middleware at stm32-mw-netx.  At the beginning, I expected by providing my own BSD addon, I could run the azure-iot. But it turns out that the BSD addon in that repository is not used by MQTT. Can you suggest how I can integrate my sockets to the azure-iot/MQTT addon?

 

Best regards,

Hongwei

This topic has been closed for replies.
Guillaume K
Guillaume KBest answer
ST Employee
Dec 20, 2024 4:41 PM UTC

If you use a 4G modem that provides its own TCP-IP stack you may have a look at Netxduo compilation flag NX_ENABLE_TCPIP_OFFLOAD. See:

https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/netx-duo/chapter3.md#tcpip-offload

of course you have to provide the offload functions.

no guarantee it works. I didn't test it.

It works at TCP-IP level, not TLS. azure-iot add-on will use netxduo's TLS functions.

Also there are some example of use of cellular modem in X-CUBE-AZURE package on st.com but it is for STM32U5 with Trustzone.

There may be examples in X-CUBE-AZURE-CELLULAR package.

if you want to have technical details about how to connect to Azure IoT without Azure SDK (with your own MQTT client and TLS), see Microsoft doc https://learn.microsoft.com/en-us/azure/iot/iot-mqtt-connect-to-iot-hub#using-the-mqtt-protocol-directly-as-a-device

also:

Implementing MQTT Communication with Azure IoT Hub... - STMicroelectronics Community

 

 

5 replies

Andrew Neil
Super User
Dec 20, 2024 2:12 PM UTC

Wouldn't it be easier to just find a generic MQTT implementation which isn't tied to a particular IP stack?

 

https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/netx-duo/index.md

https://wiki.st.com/stm32mcu/wiki/Introduction_to_NETXDUO

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
Dec 20, 2024 2:40 PM UTC

I hope to have the netXDuo azure_iot addon, which depends on its MQTT addon. I'm not sure if any generic MQTT could be used to replace the nexT Duo MQTT addon?

Andrew Neil
Super User
Dec 20, 2024 2:47 PM UTC

OK - I've edited the title to make that clearer

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Guillaume K
Guillaume KBest answer
ST Employee
Dec 20, 2024 4:41 PM UTC

If you use a 4G modem that provides its own TCP-IP stack you may have a look at Netxduo compilation flag NX_ENABLE_TCPIP_OFFLOAD. See:

https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/netx-duo/chapter3.md#tcpip-offload

of course you have to provide the offload functions.

no guarantee it works. I didn't test it.

It works at TCP-IP level, not TLS. azure-iot add-on will use netxduo's TLS functions.

Also there are some example of use of cellular modem in X-CUBE-AZURE package on st.com but it is for STM32U5 with Trustzone.

There may be examples in X-CUBE-AZURE-CELLULAR package.

if you want to have technical details about how to connect to Azure IoT without Azure SDK (with your own MQTT client and TLS), see Microsoft doc https://learn.microsoft.com/en-us/azure/iot/iot-mqtt-connect-to-iot-hub#using-the-mqtt-protocol-directly-as-a-device

also:

Implementing MQTT Communication with Azure IoT Hub... - STMicroelectronics Community

 

 

ST Employee
Dec 23, 2024 7:48 AM UTC

Hello @hongwei_lyu,

These examples might be helpful for you: x-cube-azrtos-f4/Projects/STM32F429ZI-Nucleo/Applications/NetXDuo at main · STMicroelectronics/x-cube-azrtos-f4

 

With Regards,

"If your question is answered, please close this topic by clicking ""Accept as Solution""."