Skip to main content
Associate III
Mar 16, 2024 10:06 AM UTC
Question

How to Inject Configuration Files into STM32 Target Using FileX?

Hello STM community,

I'm working on a project where I need to inject pre-configured config.ini and cacert.pem files into my STM32 target for mbedlts communication. I've gone through the STM32CubeU5 example for FileX, which demonstrates creating a file at runtime.

However, I'm unsure how to modify this example to include code that reads these configuration files from storage internal flash and then perform the necessary operations with them.

Could anyone provide guidance or share an example of how to achieve this using FileX on STM32?

https://github.com/STMicroelectronics/STM32CubeU5/tree/main/Projects/B-U585I-IOT02A/Applications/FileX

 

Thank you in advance for your help!

Best regards,

This topic has been closed for replies.

14 replies

Tesla DeLorean
Guru
Mar 16, 2024 3:25 PM UTC

Could swear you've already asked this. Put the data into a C uint8_t array, put it in it's own .H for convenience. Use pointer and sizeof() to determine location and scope content.

Perhaps if you have some level of sophistication you can put multiple files, with names, sizes, and pointers into a table/structure.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate III
Mar 16, 2024 3:31 PM UTC

Thanks for the quick response 

Is there any other alternative way to achieve this without this uint8_t array

By the way could you please give me some examples to uint8_t.

 

Pavel A.
Mar 16, 2024 4:33 PM UTC

Do you need a filesystem, besides these two files? If not: find API that takes the data from memory (pointer/array) rather than named files. If no such API, implement _open() , _read() and whatever else your libraries need to read the files rather than hauling entire filesystem package into your project.

Associate III
Mar 16, 2024 4:40 PM UTC

@Pavel A. 

I want file system.

 

Pavel A.
Mar 16, 2024 5:47 PM UTC

Great. Then you need SD card or eMMC chip, or something else. Create a filesystem image from your files, put it on the storage. Mount it. Task complete!

 

Associate III
Mar 16, 2024 5:53 PM UTC

Sorry, I don’t want to use the SD card 

I want to use flash memory for this as I am going to use the STM nucleo which having 4MB flash. 

 

Pavel A.
Mar 16, 2024 6:12 PM UTC

Then the internal flash will be the storage. Same plan.

 

Associate III
Mar 21, 2024 9:46 AM UTC

@Pavel A. 
But my Basic query is, how can I load my raw files(config.ini and cacert.pem) into the flash memory, Without using the array approch.

Pavel A.
Mar 21, 2024 4:11 PM UTC

You can, for example, just write the data file into internal flash as a binary, at a fixed address, using CubeProgrammer.

Associate III
Mar 22, 2024 10:42 AM UTC

@Pavel A. 
Sure! I successfully achieved this with the ESP32.
Now, I'm looking for guidance on how to accomplish the same task of writing data files into flash memory using CubeProgrammer. Are there specific steps, documents, or tutorials available for reference?

Pavel A.
Mar 22, 2024 1:37 PM UTC

Just open the CubeProgrammer. Connect to your MCU.

Then open the data file (you can change the suffix to .bin).

Then click on the down arrow on the right of DOWNLOAD button and enter the address on the MCU. For example 0x08001000. It should be on the boundary of the flash erase block. 

Then click on DOWNLOAD. Watch your data file programmed on the flash...