Skip to main content
BParh.1
Senior III
Oct 21, 2021 4:32 AM UTC
Solved

How to get USB stick free size in FAT file system?

Hi,

I am working to make application of USB host. At initial stage, I need to read how big is the free size of attached USB stick using the FAT file system middle ware. Can someone give me some pointer which FAT system interface I can use? I know how to mount and dismount, but not sure how to get this USB stick free size.

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
Oct 21, 2021 5:49 AM UTC

2 replies

KnarfB
KnarfBBest answer
Super User
Oct 21, 2021 5:49 AM UTC
Tesla DeLorean
Guru
Oct 21, 2021 10:15 AM UTC
void printsize(uint32_t size, char *s)
{
 if (size >= 1000000) // Storage vendor math
 printf(" %6.1lf GB %s\n", (double)size / 1000000.0, s);
 else if (size >= 1000)
 printf(" %6.1lf MB %s\n", (double)size / 1000.0, s);
 else
 printf(" %6.1lf KB %s\n", (double)size, s);
}
 
 
{
 FATFS *fs;
 DWORD fre_clust, fre_sect, tot_sect;
 
 /* Get volume information and free clusters of drive 1 */
 
 res = f_getfree("", &fre_clust, &fs);
 
 if (res != FR_OK)
 {
#ifdef DBG
 printf("res = %d f_getfree\n", res);
#endif
 return;
 }
 
 switch(fs->fs_type)
 {
 case FS_FAT12 : puts("FAT12"); break;
 case FS_FAT16 : puts("FAT16"); break;
 case FS_FAT32 : puts("FAT32"); break;
 case FS_EXFAT : puts("EXFAT"); break;
 default : puts("Unknown FAT");
 }
 
 /* Get total sectors and free sectors */
 tot_sect = (fs->n_fatent - 2) * fs->csize;
 fre_sect = fre_clust * fs->csize;
 
 /* Print the free space (assuming 512 bytes/sector) */
 printsize(tot_sect / 2, "total drive space");
 printsize(fre_sect / 2, "available");
 printsize((tot_sect - fre_sect) / 2, "used");
}

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..