Skip to main content
agalindo
Associate
Apr 5, 2022 10:32 AM UTC
Solved

How to generate .bin from web files (Web server application)

Hi everybody,

I am working with AZURE RTOS and I have implemented an HTTP web server application. I started from the example available in CubeIDE. Everything is working properly but now I need to modifiy the HTTP web page. For this, it is necessary to generate a .bin file from the .js, .css and .html files:

0693W00000LwvohQAB.pngCould somebody help me with this issue? I think it should exists a script or something like that for it.

Thanks in advance.

This topic has been closed for replies.
mattias norlander
ST Technical Moderator
Apr 7, 2022 8:57 AM UTC

Hi,

In this case I think you may find this thread interesting:

https://community.st.com/s/question/0D53W00000etOsmSAE/http-server-convert-html-file-to-c-data-array-for-in-memory-storage-does-anybody-have-a-good-example

Have a look at Vangelis answer...

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

7 replies

mattias norlander
ST Technical Moderator
Apr 6, 2022 9:14 AM UTC

Hi,

Did you start from:

X-CUBE-AZRTOS-H7\2.0.0\Projects\STM32H735G-DK\Applications\NetXDuo\Nx_WebServer

If relying on the above example then you are storing the webpage on an SD-card, relying on FileX... No bin-file should be needed.

So, I assume you are based on another example?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
agalindo
agalindoAuthor
Associate
Apr 6, 2022 9:39 AM UTC

Hi,

I started from:

X-CUBE-AZRTOS-F4\1.0.0\Projects\STM32F429ZI-Nucleo\Applications\NetXDuo\Nx_WebServer

Then, it is necessary to store the binary in the flash memory. Actually that is the best solution for my project as I don't have SD-card reader (LevelX is used as well).

Thanks.

mattias norlander
ST Technical Moderator
Apr 7, 2022 8:57 AM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
agalindo
agalindoAuthor
Associate
Apr 7, 2022 10:37 AM UTC

Thank you so much. Something like that is just what I was testing. A perl script.

agalindo
agalindoAuthor
Associate
Apr 19, 2022 3:33 PM UTC

I'm still trying to generate the web files for flash memory. web_content.bin (from web server example) has been generated in any way and I would like to know it. Does somebody know something about it?

TZhou.3
Visitor II
Apr 11, 2023 4:05 AM UTC

Just in case you are still looking for a solution, here is a script to generate raw FAT disk. 

github.com/TiejunMS/utils/tree/main/scripts/gen_raw_disk