Skip to main content
Associate II
May 7, 2026
Solved

How to enable I3C on Nucleo-H563ZI in Zephyr RTOS?

Hi Technical Support Team,
I am working with the Nucleo-H563ZI board and would like to enable the I3C interface within the Zephyr environment.
Could you provide a minimal sample project or a reference configuration (Devicetree/Kconfig) to validate the I3C host driver and I3C shell?
Thank you for your assistance.
----------------------------------------------
prj.conf
CONFIG_I3C=y
CONFIG_I3C_SHELL=y
CONFIG_I3C_STM32=y
CONFIG_USERSPACE=y
CONFIG_I3C_RTIO=y
----------------------------------------------

 

Alvin0916Best answer
Associate II
May 12, 2026

Hi Hamdi,

The minimal configuration works well.

Thank you for your support

Alvin 

4 replies

ST Technical Moderator
May 7, 2026

Hello @Alvin0916 

Please refer to the following video: 

Using I3C bus for connecting I3C and I2C sensors - Zephyr Meetup Prague

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Alvin0916Author
Associate II
May 7, 2026

Hi Saket_Om,

Could you let me know which Zephyr version this demo is implemented with?
compiler environment # Zephyr version :4.3.99
Is the arduino_i3c: &i3c1 {}; line necessary for the I3C driver to work?

Would it be possible for you to review the nucleo_h563zi.overlay?
#video's Timestamp at 10:53

------------------------nucleo_h563zi.overlay-------------------------

&i3c1 {
pinctrl-0 = <&i3c1_scl_pd12 &i3c1_sda_pd13>;
pinctrl-names = "default";
status = "okay";

clocks = <&rcc STM32_CLOCK(APB1, 23U)>,
 <&rcc STM32_SRC_HSI I3C1_SEL(2)>;
i2c-scl-hz = <400000>;
i3c-scl-hz = <6000000>;
}
-------------------------------------------ref info-----------------------------

/* /home/alvin/zephyrproject/zephyr/boards/st/nucleo_h563zi/nucleo_h563zi-common.dtsi */
&i3c1 {
	pinctrl-0 = <&i3c1_scl_pd12 &i3c1_sda_pd13>;
	pinctrl-names = "default";
	i3c-scl-hz = <12500000>;
	status = "okay";
};

&rcc {
	clocks = <&pll>;
	clock-frequency = <DT_FREQ_M(240)>;
	ahb-prescaler = <1>;
	apb1-prescaler = <2>;
	apb2-prescaler = <1>;
	apb3-prescaler = <2>;
};

/* /home/alvin/zephyrproject/zephyr/dts/arm/st/h5/stm32h5.dtsi */
i3c1: i3c@40005c00 {
compatible = "st,stm32-i3c";
reg = <0x40005c00 0x400>;
interrupts = <123 0>, <124 0>;
interrupt-names = "event", "error";
#address-cells = <3>;
#size-cells = <0>;
clocks = <&rcc STM32_CLOCK(APB1, 23)>;
resets = <&rctl STM32_RESET(APB1L, 23)>;
zephyr,pm-device-runtime-auto;
status = "disabled";
};

rcc: rcc@44020c00 {
			compatible = "st,stm32h5-rcc";
			clocks-controller;
			#clock-cells = <2>;
			reg = <0x44020c00 0x400>;

			rctl: reset-controller {
				compatible = "st,stm32-rcc-rctl";
				#reset-cells = <1>;
			};
		};

 

T_Hamdi
ST Employee
May 8, 2026

Hello @Alvin0916 

Yes —arduino_i3c: &i3c1 {};  is not necessary for the I3C driver to work.

For your overlay, the simple recommended version is:

&i3c1 {
 i2c-scl-hz = <400000>;
 i3c-scl-hz = <6000000>;
};

&i3c1 is already enabled in nucleo_h563zi-common.dtsi, so you do not need to repeat the following:

pinctrl-0 = <&i3c1_scl_pd12 &i3c1_sda_pd13>;
pinctrl-names = "default";
status = "okay";

I also suggest removing the clocks line for now, unless you have a confirmed reason to override it.

with regrads,

Hamdi

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question.Hamdi Teyeb"
Alvin0916AuthorBest answer
Associate II
May 12, 2026

Hi Hamdi,

The minimal configuration works well.

Thank you for your support

Alvin