Skip to main content
Associate II
Oct 27, 2024 2:14 PM UTC
Question

How to enable I2C - STM32F411

how to activate I2C
Good morning
I'm trying to make a project that requires the I2C1 bus work
if I load the compiled project on arduino
from debug the application crashes because it can't read the EEPROM on RTC
I've read various documents but I can't understand how to activate the bus on the STMF411 processor
I'm quite new to STM
with esp32 there are no problems
here it seems more complicated to me

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
Oct 27, 2024 3:53 PM UTC

Yes, programming hardware frequently more complicated than presented by Arduino where someone else has worked out the drivers and libraries

The 7-bit Slave Address on STM32 is the High Order 7-bits, not the Low Order. So frequently (SlaveAddr << 1) in translation/conversion.

Look at the documentation for the IC you are connecting, usually sets forth the expectations.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MOBEJ
ST Employee
Oct 28, 2024 11:04 AM UTC

Hello @ezioall , 

You can refer to this example from STMicroelectronics: I2C_TwoBoards_ComPolling Example. This example demonstrates how to handle I2C communication between two boards, which might be helpful for your case involving STM32 and Arduino.

Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ezioallAuthor
Associate II
Oct 28, 2024 11:14 AM UTC

hi

Il MOBEJE
this code should be fine
but i have to insert my code which is composed of several .H files and the src folder
i will have to study a little

ezioallAuthor
Associate II
Oct 28, 2024 11:17 AM UTC

hi  Il MOBEJE
this code should be fine
but i have to insert my code which is composed of several .H files and the src folder
i will have to study a little