Skip to main content
mcen
Associate
Aug 8, 2021 6:44 AM UTC
Question

How to coexist Fatfs with low level Nand flash reading and writing in UC-OSiii?

I'm using STM32F415VG, on which we built uc-osIII, I've built a Fatfs on nand flash, unfortunately, we had to use a block at the end of low-level nand flash read and write. How can I change the size of Fatfs and realize that this low-level function coexists with the file system at the same time, can I realize it?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Aug 8, 2021 3:03 PM UTC

The large erase block size of NAND memories is ill-suited to MCU with limited RAM resources.

Do you have to use FatFS? Could you use something more incremental / journalling ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..