Skip to main content
Jnana Panuganti
Associate II
February 8, 2017
Question

How to calibrate the DACs on STM32 using the HAL library ?

  • February 8, 2017
  • 1 reply
  • 3372 views
Posted on February 08, 2017 at 19:25

Hello,

I am using the the HAL library for calibrating the DAC on STM32L4.

I read the documentation for  DAC on page 286 (DOCID027704 Rev 4) in HAL L4 user manual. I am still confused about how to correctly use the HAL DAC calibration APIs.

My question is how does the 

HAL_DACEx_SelfCalibrate() API work? Does it automatically apply the trimming offset? 

or do I also need to use the APIs below?

HAL_DACEx_GetTrimOffset()

HAL_DACEx_SetUserTrimming()

If yes should I be manually adding the TrimOffset before making a call to 

HAL_DAC_SetValue, s

omething like below?

trim_offset = HAL_DACEx_GetTrimOffset(&hdac1, DAC_CHANNEL_2)

HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_2, DAC_ALIGN_8B_R, input_data + trim_offset )?

Just for reference I have posted my current code below.

Below is my current calibration function:

void DAC_SelfCalibrate(void)

{

   DAC_ChannelConfTypeDef sConfig;

   sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;

   sConfig.DAC_Trigger = DAC_TRIGGER_NONE;

   sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;

   sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_DISABLE;

   sConfig.DAC_UserTrimming = DAC_TRIMMING_USER;

   //Calibrate DAC channel 1

   if (HAL_DACEx_SelfCalibrate(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)

   {

      Error_Handler();

   }

   //Calibrate DAC channel 2

   sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_DISABLE;

   if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_2) != HAL_OK)

   {

      Error_Handler();

   }

}

and here is my  code to set the DAC

int set_dac_val(uint8_t input_index, uint8_t input_data)

{

   //set dac channel 1

   if(input_index==0) {

      HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_8B_R, input_data);

   //set dac channel 2

   }

   else if(input_index==1)

   {

      HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_2, DAC_ALIGN_8B_R, input_data);

   }

   return 0;

}

Below is my sequence of calls for initialization.

MX_DAC1_Init(); 

DAC_SelfCalibrate();

HAL_DAC_Start(&hdac1, DAC_CHANNEL_1);

HAL_DAC_Start(&hdac1, DAC_CHANNEL_2);

I have a similar question about HAL based ADC calibration and usage of calibration factor. I will post that under a separate thread.

Thanks!

#hal #dac #calibration
This topic has been closed for replies.

1 reply

ST Technical Moderator
February 14, 2017
Posted on February 14, 2017 at 15:14

Hello

Panuganti.Jnana.002

‌,

The

useofthe HAL DAC calibration

depends on your needs and your use case defined.

The settings can be figured out using self calibration handled by HAL_DACEx_SelfCalibrate whichruns automatically the calibration and enables the user trimming mode with fresh calibration results.

You can refer to the 'DAC channel buffer calibration' in your reference manual, it may help you on DAC calibration, on user trimming calibration and about the function to use for an N-bit DAC.

Maybe the working example in the STM32CubeL4 firmware package can help you to implement your project:

STM32Cube_FW_L4_V1.6.0\Projects\STM32L476G_EVAL\Examples\DAC

Best Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks