how i can recover the state of HAL_Init () with stm32f4
HAL_StatusTypeDef HAL_Init( void )
{ HAL_StatusTypeDef statue;
/* Configure Instruction cache through ART accelerator */
#if (ART_ACCLERATOR_ENABLE != 0)
__HAL_FLASH_ART_ENABLE();
#endif /* ART_ACCLERATOR_ENABLE */
/* Configure Flash prefetch */
#if (PREFETCH_ENABLE != 0U)
__HAL_FLASH_PREFETCH_BUFFER_ENABLE();
#endif /* PREFETCH_ENABLE */
/* Set Interrupt Group Priority */
HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* Use systick as time base source and configure 1ms tick (default clock after Reset is HSI) */
HAL_InitTick(TICK_INT_PRIORITY);
/* Init the low level hardware */
HAL_MspInit();
/* recuperer function status */
return HAL_OK ;