Skip to main content
Wisse Pielage
Associate II
Feb 20, 2017 3:46 PM UTC
Solved

How does the UART bootloader responds feedback?

Posted on February 20, 2017 at 16:46

Hi,

We are designing a project where we would like to use the default bootloader on a LIN connection.

The MCU we plan on using is the STM32F030RC, with external LIN-driver.

The LIN-driver merges Tx & Rx, so everything send will be visible on the Rx.

How does the UART bootloader respond to its own ack/nack or data?

Does it get in a loop where it nack's its own data because it is not a known command?

Thanks in advance!

#stm32f030 #lin #bootloader
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Feb 20, 2017 4:59 PM UTC
Posted on February 20, 2017 at 17:59

It doesn't expect feedback, and will likely not function well if that occurs, either at the command and parameter level, or data.

The firmware times the 0x7F at 7E1 pattern, and responds with a 0x79

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

Oliver Beirne
Associate II
Feb 20, 2017 3:56 PM UTC
Posted on February 20, 2017 at 16:56

Hello

I have moved your question to the

https://community.st.com/community/stm32-community/stm32-forum?sr=search&searchId=79af816d-ae78-426a-b02f-5a92a9337c2e&searchIndex=0

‌ where someone should be able to assist you.

Thanks

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Feb 20, 2017 4:59 PM UTC
Posted on February 20, 2017 at 17:59

It doesn't expect feedback, and will likely not function well if that occurs, either at the command and parameter level, or data.

The firmware times the 0x7F at 7E1 pattern, and responds with a 0x79

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Wisse Pielage
Associate II
Feb 21, 2017 9:44 AM UTC
Posted on February 21, 2017 at 09:44

Thanks for your fast response!

Looks like I have to write my own, or change the plans!

Tesla DeLorean
Guru
Feb 21, 2017 5:22 PM UTC
Posted on February 21, 2017 at 17:22

My advice on STM32 designs is not to do odd things with standard interfaces used for system loader functionality. ie have the USART go to an RS232 port or headers, don't connect it to a modem or GPS receiver

The F030 is likely pin/usart constrained, so I can see that as being an issue.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..