Skip to main content
jet_socks
Visitor II
March 2, 2021
Question

How do you write/read from pins Pxx_C ?

For example, when using the HAL drivers to write to a pin you would normally write:

 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_RESET);

But, how would you do that using PA1_C, for instance?

Thank you.

This topic has been closed for replies.

3 replies

Pavel A.
March 2, 2021

What is PA1_C? Pins of port A are named PA0-PA15. Pins of port C are named PC0-PC15.

-- pa

Uwe Bonnes
Chief
March 2, 2021

These are special bond options on some big BGA packages.

waclawek.jan
Super User
March 3, 2021

The functionality is completely split between Pxx and Pxx_C, so only to one of them is the GPIO connected, see pin table in datasheet. Unless you switch on the switch which connects the two internally, you cannot use GPIO to read/write the state of other.

JW