Skip to main content
arnold_w
Senior II
Jun 20, 2022 5:18 PM UTC
Question

How do I reset the internal USB state machine correctly when something USB-related goes wrong?

I'm working with the Nucleo-64 development board with an STM32L476 microcontroller and I'm using the USB source code that STM32CubeMX has generated for me. Every once in a while something unpredictable happens, e.g. the user unplugs the USB-cable in the middle of a packet or the microcontroller attempts to send something before the cable has been plugged in properly. When something goes wrong, I would like to have a reliable way to abort all ongoing transmissions/receptions and reset the USB state machine, without having to call __USB_FORCE_RESET or MX_USB_DEVICE_Init(). What would such a function look like? Right now I call these functions:

USB_FlushRxFifo(USB_OTG_FS);
USB_FlushTxFifo(USB_OTG_FS, 15);

but I can see that ((USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData)->TxState is still 1 in some error cases. Can anybody please help me?

This topic has been closed for replies.