Skip to main content
vicfer89
Associate II
Aug 30, 2021 8:59 PM UTC
Question

How can I use sockets with LWIP and FreeRTOS?

I am trying to use Sockets under FreeRTOS. Currently can send data over UDP using netconn, but sockets only send information when two netconn messages are sent previous to the socket one. If some of the netconn_sendto(...) functions is commented, sendto stops working.

void UDP_Send_Thread(void)
{
	// Creamos estructuras de datos necesarias para los envíos
	 struct netconn *conn;
	 struct netbuf *outbuf;
	 u8_t dataraw[] = "Hola UDP RTOS\n";
 
	 // Generamos IP para envío de datos
	 ip_addr_t ipto;
	 IP4_ADDR(&ipto,172,16,0,2);
 
	 // Creamos conexión UDP con netconn
	 conn = netconn_new(NETCONN_UDP);
 
	 int s = socket(AF_INET, SOCK_DGRAM, 0);
	 struct sockaddr_in addr, cliaddr;
	 memset(&addr, 0, sizeof(addr));
	 memset(&cliaddr, 0, sizeof(cliaddr));
	 addr.sin_family = AF_INET;
	 addr.sin_addr.s_addr = IP_ADDR_ANY;
	 addr.sin_port = htons(60000);
 
	 cliaddr.sin_family = AF_INET;
	 cliaddr.sin_addr.s_addr = inet_addr("172.16.0.2");
	 cliaddr.sin_port = htons(49002);
 
	 int b = bind(s, (const struct sockaddr *) &addr, sizeof(addr));
 
	 // Creamos buffer para envío de datos de tipo netbuf
	 outbuf = netbuf_new();
	 // referenciamos cadena de texto al buffer
	 netbuf_ref(outbuf, dataraw, sizeof(dataraw));
 
	 for(;;)
	 {
		 // Enviamos datos
		 netconn_sendto(conn, outbuf, &ipto, 49000);
		 netconn_sendto(conn, outbuf, &ipto, 49001);
		 osDelay(500);
		 // Indicamos con un LED que el envío se ha hecho (parpadeo)
		 sendto(s, dataraw, strlen(dataraw), MSG_DONTWAIT, (const struct sockaddr *) &cliaddr, sizeof(cliaddr));
		 HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
		 osDelay(500);
	 }
}

Can somebody help me regarding with this issue? I am trying to learn how to use all Raw, Sockets and Netconn LWIP.

Thanks in advance.

This topic has been closed for replies.

1 reply

vicfer89
vicfer89Author
Associate II
Sep 3, 2021 4:25 PM UTC

I solved the issue... Following code works fine sending standalone Sockets messages and Messages in conjunction with netconn

int Eth_UDP_Init(int port)
{
	int on = 1; // On value for SO_BROADCAST
 
	struct sockaddr_in sockin;
 
	int sd = socket(AF_INET, SOCK_DGRAM, 0); // Init a Socket descriptor
	memset((uint8_t *) &sockin, 0, sizeof(sockin)); // Reset all sockin values to zero
	sockin.sin_family = AF_INET;
	sockin.sin_port = htons(port); // htons() converts int to host port information
	/* Bind a name to the socket */
	if( bind(sd, (struct sockaddr*) &sockin, sizeof(sockin)) == -1 )
	{
		printf("Error on socket binding: %d \n", port);
		return 0;
	}
	printf("Socket binded for port %d \n", port);
 
	/* Socket options:
	 * 	- SOL_SOCKET: To manipulate options at "Socket" level
	 * 	- SO_BROADCAST: To send data to more than one destination */
	setsockopt(sd, SOL_SOCKET, SO_BROADCAST, &on, sizeof(on));
 
	return sd;	// returns socket descriptor
}
 
long UDP_Send(int sd, char *buf, int buflen, char *ipdest, int portdest)
{
 
	struct sockaddr_in servaddr; // Destination descriptor
 
	servaddr.sin_family = AF_INET;
	servaddr.sin_port = htons(portdest);
	servaddr.sin_addr.s_addr = inet_addr(ipdest);
 
	return sendto(sd, buf, buflen, 0, (struct sockaddr*) &servaddr, sizeof(servaddr) );	// send to an specific source
 
}
 
void UDP_Send_Thread(void)
{
	// Creamos estructuras de datos necesarias para los envíos
	 struct netconn *conn;
	 struct netbuf *outbuf;
	 int sd, sd2;
	 u8_t dataraw[] = "Hola UDP RTOS\n";
 
	 // Generamos IP para envío de datos
	 ip_addr_t ipto;
	 IP4_ADDR(&ipto,172,16,0,2);
 
	 // Creamos conexión UDP con netconn
	 conn = netconn_new(NETCONN_UDP);
	 sd = Eth_UDP_Init(60000);
	 sd2 = Eth_UDP_Init(50000);
 
	 // Creamos buffer para envío de datos de tipo netbuf
	 outbuf = netbuf_new();
	 // referenciamos cadena de texto al buffer
	 netbuf_ref(outbuf, dataraw, sizeof(dataraw));
 
	 for(;;)
	 {
		 // Enviamos datos
		 netconn_sendto(conn, outbuf, &ipto, 49000);
		 netconn_sendto(conn, outbuf, &ipto, 49001);
		 UDP_Send(sd, dataraw, strlen(dataraw), "172.16.0.2", 60001);
		 UDP_Send(sd2, "Hola SD2", strlen("Hola SD2"), "172.16.0.2", 60001);
		 osDelay(500);
		 // Indicamos con un LED que el envío se ha hecho (parpadeo)
		 HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);
		 osDelay(500);
	 }
}

Hope can help you to face issues like mine

:)