Skip to main content
Kyoun.4
Associate
Aug 24, 2021 7:50 AM UTC
Solved

How can i switch gpio function from USB to normal GPIO?

I set stm32f401 to use USB and deinit USB to dP/dN to use normal GPIO.

But I can not control dP/dN for GPIO.

How can I switch GPIO function from USB to normal GPIO?

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Aug 24, 2021 10:34 AM UTC

What is this, SPL?

I don't use SPL nor Cube. As I've said, make sure OTG_GCCFG.PWRDWN gets cleared. Read the post I've linked to above, and the posts linked from there.

JW

7 replies

TDK
Aug 24, 2021 8:28 AM UTC

HAL_GPIO_Init can be used to set the target mode, same as any other GPIO pin. Ensure the clock is enabled. CubeMX will generate the code for you.

USB pins are not set up in USB mode by default.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Kyoun.4
Kyoun.4Author
Associate
Aug 24, 2021 10:25 AM UTC

I set the following process to switch USB DP/DN port to normal GPIO.

But​ it still in DP/DN mode and can not control as normal GPIO.

 // USB Device Off (DP/DN Port Off ???)

  if (USBH_Stop(&hUsbHostFS) != USBH_OK)

  {

   Error_Handler();

  }

​

  if (USBH_DeInit(&hUsbHostFS) != USBH_OK)

  {

   Error_Handler();

  }

​

  // DP/DN Port GPIO Input Mode

  GPIO_InitTypeDef GPIO_InitStruct = {0};

​

  GPIO_InitStruct.Pin = USB_DN_Pin|USB_DP_Pin;

  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

​

  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

waclawek.jan
Super User
Aug 24, 2021 9:27 AM UTC

I don't know what is "deinit USB", but in 'F407 - and most probably also in 'F401 - USB PHY overrides the GPIO settings, so you have to switch it off by clearing OTG_GCCFG.PWRDWN.

This is not documented by ST.

JW

Kyoun.4
Kyoun.4Author
Associate
Aug 24, 2021 10:24 AM UTC

I set the following process to switch USB DP/DN port to normal GPIO.

But​ it still in DP/DN mode and can not control as normal GPIO.

 // USB Device Off (DP/DN Port Off ???)

  if (USBH_Stop(&hUsbHostFS) != USBH_OK)

  {

   Error_Handler();

  }

​

  if (USBH_DeInit(&hUsbHostFS) != USBH_OK)

  {

   Error_Handler();

  }

​

  // DP/DN Port GPIO Input Mode

  GPIO_InitTypeDef GPIO_InitStruct = {0};

​

  GPIO_InitStruct.Pin = USB_DN_Pin|USB_DP_Pin;

  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

​

  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

Kyoun.4
Kyoun.4Author
Associate
Aug 24, 2021 10:00 AM UTC

I set the following process to switch USB DP/DN port to normal GPIO.

But​ it still in DP/DN mode and can not control as normal GPIO.

 // USB Device Off (DP/DN Port Off ???)

  if (USBH_Stop(&hUsbHostFS) != USBH_OK)

  {

   Error_Handler();

  }

​

  if (USBH_DeInit(&hUsbHostFS) != USBH_OK)

  {

   Error_Handler();

  }

​

  // DP/DN Port GPIO Input Mode

  GPIO_InitTypeDef GPIO_InitStruct = {0};

​

  GPIO_InitStruct.Pin = USB_DN_Pin|USB_DP_Pin;

  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

​

  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

waclawek.jan
waclawek.janBest answer
Super User
Aug 24, 2021 10:34 AM UTC

What is this, SPL?

I don't use SPL nor Cube. As I've said, make sure OTG_GCCFG.PWRDWN gets cleared. Read the post I've linked to above, and the posts linked from there.

JW

Kyoun.4
Kyoun.4Author
Associate
Aug 25, 2021 3:22 AM UTC

Thanks!

Works well.