How can I send more than 3 CAN messages in a row using HAL library
I am using the latest HAL library to transmit CAN messages using interrupts. I am aware of the 3 mailboxes limitation but I would like to know if someone had implemented a queue system that transmit most of the CAN messages.
I tried to follow the HAL_StatusTypeDef HAL_CAN_Transmit_IT(CAN_HandleTypeDef* hcan) function.
So putting counters on every return of this function equals 1 vs the TX interrupt, my counters are not matching.
To enable the TX interrupts, I simply set:
HAL_NVIC_SetPriority(CAN1_TX_IRQn,3, 0);
HAL_NVIC_EnableIRQ(CAN1_TX_IRQn);Do I need to set another flag? from my understanding, using the HAL_CAN_Transmit_IT will generate an interrupt, is that correct?
#hal #can