Skip to main content
sdavi.9
Associate II
Mar 26, 2019 9:28 PM UTC
Solved

How and where do I write my interrupt function? Working with CubeMX on a Nucleo

Hi,

I'm starting to work with a Nucleo-64 with a STM32F072RBT6.

I'm reading these documents and not really understandign them:

https://www.st.com/content/ccc/resource/technical/document/user_manual/2f/77/25/0f/5c/38/48/80/DM00122015.pdf/files/DM00122015.pdf/jcr:content/translations/en.DM00122015.pdf

https://www.st.com/resource/en/datasheet/stm32f072c8.pdf

I configured the Timer1 correctly. I start it with these lines of code :

 HAL_TIM_PWM_Start_IT(&htim1, TIM_CHANNEL_1); //Start the channel in interrupt mode

 HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_4); //Start this channel with no interrupt

I tested with a scope that these few lines work:

 while (1)

 {

  /* USER CODE END WHILE */

 HAL_Delay(1000);

 TIM1->CCR4 = 1500;

 TIM1->CCR1 = 1500;

 HAL_Delay(1000);

 TIM1->CCR4 = 500;

 TIM1->CCR1 = 500;

  /* USER CODE BEGIN 3 */

 }

My question is how (what syntax ) do I write the code I want to put in the interrupt routine ?

Am I correct to assume that I should write it in this file : stm32f0xx_it.c

(It says so in the file.... so i'm pretty sure about that part.)

In an Atmel chip, I would just write:

ISR(TIMER1_OVF_vect){

//my code in here

{

What is it for an STM?

I read chapter 11.1.2 Initialization and de-initialization functions where these function are described breifly.

HAL_NVIC_SetPriority()

HAL_NVIC_EnableIRQ()

HAL_NVIC_DisableIRQ()

HAL_NVIC_SystemReset()

HAL_SYSTICK_Config()

I also read chapter 11.1.3 for the rest of the NVIC functions

It says  (For the complete STM32 Devices IRQ Channels list, please refer to stm32f0xx.h file) I found said file. but I didn't find the list of IRQ Channels.

But whe it says  (For the complete STM32 Devices IRQ Channels list, please refer to the appropriate CMSIS device file (stm32f0xxxx.h)) I did not find that file.

I've dealt with IRQs and different IRQ priority in the past. But i don't seem to understand them in the ARM architecture.

Thank you for helping a someone new to STM and ARMs in general.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Mar 26, 2019 11:54 PM UTC

The interrupts will all be listed in the vector table in startup.s

For coverage of NVIC, perhaps try Joseph Yiu's Essential Cortex Mx series.

The interrupt handlers are often live in stm32f0xxx_it.c

In the HAL model your TIM1_IRQHandler() typically calls back into the HAL, and it in turn calls the routine you provided as a callback. This is highly circuitous, and you can chose to do it differently.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Mar 26, 2019 11:54 PM UTC

The interrupts will all be listed in the vector table in startup.s

For coverage of NVIC, perhaps try Joseph Yiu's Essential Cortex Mx series.

The interrupt handlers are often live in stm32f0xxx_it.c

In the HAL model your TIM1_IRQHandler() typically calls back into the HAL, and it in turn calls the routine you provided as a callback. This is highly circuitous, and you can chose to do it differently.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
sdavi.9
sdavi.9Author
Associate II
Apr 4, 2019 3:07 PM UTC

Thanks,

I managed to get Cube MX to generate the emtpy interrupt fonction

TIM1_CC_IRQHandler(void)