Skip to main content
HBrun.1
Associate
Jul 12, 2021 3:32 PM UTC
Question

Hi, i want to work with my STM32F4 Discovery Board in a stand alone mode. I supply the board with external 5 V like described in the manual. But its works only when my development environment is connected via USB. How can i work in a stand alone mode

..

This topic has been closed for replies.

3 replies

waclawek.jan
Super User
Jul 12, 2021 8:30 PM UTC
Tesla DeLorean
Guru
Jul 12, 2021 8:49 PM UTC

If there is a solder-bridge for NRST, consider removing that.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
HBrun.1
HBrun.1Author
Associate
Jul 18, 2021 7:53 PM UTC

Hi Jan, hi Tesla,

thank you for ur answers.

The Problem is solved. Indeed there is a solid bridge between NRST and the on-board-developer (Pin T_NRST) at the buttom side.

I dont understand such a design because in such a case i await a jumper.

To close the SB again its fortunately possible to connect both pins on connectors at the top side.

:grinning_face: