Skip to main content
svii
Associate III
Oct 23, 2019 8:21 AM UTC
Solved

Hi, I'm using stm32L073Rz , need to know how to configure it as a usb memory device, no demo examples are available for usb memory stick for this chip , i used cubemx to generate code for usb memory class and ran it.

It does not work , it gets detected as unknown device,what am i missing , should i add something more to cube mx generated code. Thanks.

This topic has been closed for replies.
David SIORPAES
David SIORPAESBest answer
ST Employee
Oct 23, 2019 2:27 PM UTC

There's a MSC example available in the Cube-L0 package here: STM32Cube_FW_L0_V1.11.2\Projects\STM32L073Z-EVAL\Applications\USB_Device\MSC_Standalone

3 replies

David SIORPAES
David SIORPAESBest answer
ST Employee
Oct 23, 2019 2:27 PM UTC

There's a MSC example available in the Cube-L0 package here: STM32Cube_FW_L0_V1.11.2\Projects\STM32L073Z-EVAL\Applications\USB_Device\MSC_Standalone

svii
sviiAuthor
Associate III
Oct 25, 2019 10:32 AM UTC

hi, thanks i did refer the example above , for my own code generated by cubemx, their is no difference much implementation is the same, i have a custom board with a nucleo -L073R mcu on it , do not have the stm32L073z-eval board , as i had posted earlier the usb is detecting as an unknown device , but why can't it register it as stm Mass Storage device as give in the usbd_desc.c file . Have i missed something .Thanks .

svii
sviiAuthor
Associate III
Oct 28, 2019 11:28 AM UTC

Hi Thanks , issue was due to clock, thanks for the reference example.