Skip to main content
FOzat
Associate II
Nov 29, 2022 8:35 PM UTC
Question

Hi, I'm trying to implement stm32f7 discovery cube package example. (USB Mass Storage) in High speed mode. I inserted microSD card into slot. after i build and load the image into the memory , i can see the files inside microsd card.

but when i start to copy and paste these files to another location . i can not get the true speed. (while writing reading) I mean I choose HS mode (60Mb/s) but transfer speed is too low. I made everything in the readme.txt file. but i can not implement this fw. example (high speed mode). Can anyone to help me??

This topic has been closed for replies.

2 replies

FOzat
FOzatAuthor
Associate II
Nov 29, 2022 8:46 PM UTC

File Transfer speed is 1.5 Mb/s .. I mean HS mode is not active. but i had alread load the image. (stmcubef7 cube package USB Device MSC Standalone ). Anyone to navigate ??

I used Keil uVision.

STM32f7 discovery board.

FOzat
FOzatAuthor
Associate II
Dec 13, 2022 9:46 AM UTC

No body is here to help me ??