Skip to main content
baptor
Associate III
Jan 11, 2022 2:37 PM UTC
Question

Hi,I am using the STM32H757(master) to load code into flash of another STM32H757(slave). The slave is in bootloader mode ( SPI ). Question 1: Does somebody has a driver for the master side to read/write into slave, especialy option bytes? Thank you

..

This topic has been closed for replies.

1 reply

baptor
baptorAuthor
Associate III
Jan 11, 2022 2:40 PM UTC

Question 2 : When the Go command is issued from the master, ( set pointer to start adress of loaded code in slave), what is the core that will start from this adress ( CM4 or CM7 ) ? I dont understant how it is managed.

thank you