Skip to main content
APANT.11
Visitor II
Oct 17, 2021 2:43 AM UTC
Question

Hi, I am considering STM32H725 series microcontroller in a design. 1. Can RTL8201F ethernet PHY from Realtek be used with STM32H725 series microcontroller? 3. Does STM32H725 series has necessary libraries for Realtek Ethernet PHY ICs.

..

This topic has been closed for replies.

2 replies

TDK
Oct 17, 2021 3:29 PM UTC

1. STM32H7 supports both RMII and MII connection to PHY. The RTL8201F supports both of these types. So yes.

3. Once configured, the PHY should be transparent. There aren't PHY-specific things needed. STM32H7 library has support for LwIP for various ethernet communication protocols. There are examples.

https://community.st.com/s/article/How-to-create-project-for-STM32H7-with-Ethernet-and-LwIP-stack-working

"If you feel a post has answered your question, please click ""Accept as Solution""."
Piranha
Principal III
Oct 20, 2021 11:20 AM UTC

All typically required things are common, except for two - the speed and duplex status bits of the auto-negotiation result are PHY specific and located in PHY specific register.