Skip to main content
Visitor II
Jul 1, 2025 4:59 PM UTC
Question

Help with FileX/LevelX Implementation on STM32U585AII6Q with NOR Flash (IS25LP064D)

Hello Microsoft Community,

I’m currently working on implementing a file system using FileX and LevelX on external NOR Flash (IS25LP064D) connected to the STM32U585AII6Q board.

Flash Memory Specifications:

    • Sector Size: 4 KB
    • Block Size: 32 KB / 64 KB
    • Total Flash Size: 64 Mbit / 8 MB
    • Page Size: 256 bytes

Requirement:

I need to create a .txt log file using FileX and once the file reaches 100 KB, it should be deleted and a new file created in its place.

Media Initialization Parameters Used:

    • Total clusters: 300
    • Bytes per sector: 512
    • Sectors per cluster: 8
    • Hidden sectors: 0
    • Heads and sectors per track: 1
    • Number of FATs: 1

Issue:

When writing logs using FileX, I receive a FX_IO_ERROR after a few logs are written—even though there is still available space on the flash.

My Questions:

  1.   What are the correct parameters to pass to fx_media_format() for this NOR flash setup (e.g., sector size, cluster size, number of FATs)?
  2. Is there a formula or guideline for determining these parameters when using NOR flash with FileX/LevelX?
  3. I was able to initialize the media with a size of 150 KB—what is the minimum required size for successful media initialization

 

Thanks

Shilpa

 

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Jul 2, 2025 2:18 AM UTC

You should use 4KB sectors. 1 per cluster.

Instrument the IO layer to understand why it fails.

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ST Technical Moderator
Jul 2, 2025 1:34 PM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om