Skip to main content
RBela.1
Visitor II
Feb 10, 2022 8:43 PM UTC
Question

Hello, I am wanting to do a firmware upgrade on a STM32H7 processor through a USB connected to another microprocessor(Such as an Eval board). Are there any examples or libraries for firmware that will run on the Eval board which will upgrade the STM3

..

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Feb 10, 2022 9:45 PM UTC

Not sure there is a DFU HOST, but there is a DEVICE

STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\USB_Device\DFU_Standalone

You could perhaps have the donor device be an MSC DEVICE, and use the FW UPGRADE firm READ file/data content that way.

STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\USB_Device\MSC_Standalone

STM32Cube_FW_H7_V1.8.0\Projects\STM32H743I-EVAL\Applications\USB_Host\FWupgrade_Standalone

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..