Skip to main content
RIvan.1
Associate II
Jan 11, 2020 4:31 PM UTC
Solved

Hello. Can't find: - STM32 Standard Peripheral Libraries, for STM32H7, could You help me with this?

..

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 11, 2020 5:03 PM UTC

ST hasn't supported SPL in several years, no official SPL exists for the H7

They have a LL (Low Level) library, and others DIY subsets to suit their own needs.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

7 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Jan 11, 2020 5:03 PM UTC

ST hasn't supported SPL in several years, no official SPL exists for the H7

They have a LL (Low Level) library, and others DIY subsets to suit their own needs.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RIvan.1
RIvan.1Author
Associate II
Jan 14, 2020 3:38 PM UTC

Thank you for the information. I can't find the LL libraries, could you give a link to these libraries?

Tesla DeLorean
Guru
Jan 14, 2020 4:39 PM UTC

CubeH7, unpack the archive, should be libraries and examples using LL

https://www.st.com/en/embedded-software/stm32cubeh7.html

STM32Cube_FW_H7_V1.5.0\Projects\NUCLEO-H743ZI\Examples_LL\DAC\DAC_GenerateWaveform_TriggerHW

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RIvan.1
RIvan.1Author
Associate II
Jan 14, 2020 5:14 PM UTC

I have a stm32cube MCU Package for STM32H7 series1.6.0 connected, but CubeMX is Advanced Settings, I can't switch GPIO, RCC, Cortex_M7... from the HAL library to the LL library.

Tesla DeLorean
Guru
Jan 14, 2020 6:34 PM UTC

CubeMX doesn't support SPL either, I'm not using it. The CubeH7 trees have examples and templates, should be able to DIY from your tool-chain of choice.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
GIkar
Associate III
Jan 14, 2020 9:26 PM UTC

In CubeMX is the HAL standart for LL you have to change what you want code in LL in the Project settings.

fbar
Senior
Jan 17, 2020 1:29 AM UTC

I asked the same a long time ago: https://community.st.com/s/question/0D50X0000BMGMiDSQX/very-incomplete-support-for-stm32h743-ll-libraries-in-stm32cubeide

It looks like ST enabled LL code generation as promised in the 1.60 version of the H7 firmware. After enabling the peripherals you need, in Project Manager / Advanced Settings, you can choose HAL or LL code generation for each peripheral (minus peripherals like USB where due to how complex the code is, only HAL code generation is supported). Simply click on where it says HAL and you will see a drop down with either HAL or LL I tried GPIO, RCC, Cortex_M7, ADC, UART, I2C and SPI, and all are available either as LL or HAL