Skip to main content
LOGU
Associate II
Dec 23, 2020 10:50 AM UTC
Solved

Has anyone a working 1-bit SDIO FATFS example with STM32f207VE?

I would like to use SDIO with 1 bit mode with FatFS. I use STM32F207VE MCU. The SD card is a 16 GB SanDisk.

Version of STM32CubeMX is 6.1.1, firmware version is STM32Cube FW_F2 V1.9.2.

FATFS R0.11 version used.

When I generate SDIO with 1 bit mode it is not working. Function 'f_open' is returning with error code: 12 which is 'FR_NOT_ENABLED' and f_read return with error code 9, which is 'FR_INVALID_OBJECT'

// code

while(1)

{

retSD=f_mount(&SDFatFS, SDPath, 1);

HAL_Delay(20);

if(resSD == 0)

{

HAL_Delay(20);

retSD = f_open(&SDFile, "HL.txt", FA_READ);

HAL_Delay(200);

retSD = f_read(&SDFile, array,sizeof(array),bytesread);

HAL_Delay(200);

f_close(&SDFile);

}

}

help me how can I solve this.

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 23, 2020 5:43 PM UTC

You could waste the best part of forever digging bugs out of machine generated code.

I'd suggest this as a working basis for a port to your platform

STM32Cube_FW_F2_V1.9.0\Projects\STM322xG_EVAL\Applications\FatFs\FatFs_uSD

I'd also upgrade to more current FATFS that doesn't have the bugs in the ones ST distributes.

Don't mount in a loop. Mount once. Validate the functionality of DISKIO routines.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

3 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Dec 23, 2020 5:43 PM UTC

You could waste the best part of forever digging bugs out of machine generated code.

I'd suggest this as a working basis for a port to your platform

STM32Cube_FW_F2_V1.9.0\Projects\STM322xG_EVAL\Applications\FatFs\FatFs_uSD

I'd also upgrade to more current FATFS that doesn't have the bugs in the ones ST distributes.

Don't mount in a loop. Mount once. Validate the functionality of DISKIO routines.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LOGU
LOGUAuthor
Associate II
Dec 24, 2020 1:28 PM UTC

thank you tesla delorean,

i will check.

ST Technical Moderator
Jan 8, 2021 7:57 AM UTC

Hello @LOGU​ ,

Do you have still this problem to solve?

Did you follow the recommendation suggested by @Community member​ ? If his answer resolve your issue, please mark it as Best answer by clicking on "Select as Best".  This will help other users find this solution more quickly.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks