Skip to main content
bureau
Associate II
April 24, 2026
Question

HardFault_Handler() after MxCube project regeneration by using ST Example project

Hello

Currently I am working with NUCLEO-N657X0-Q by using 

  • STM32CubeIDE_2.1.1 
  • STM32Cube_FW_N6_V1.3.0
  • MxCube v6.17.0

Trying to investigate and migrate CDC ACM feature in to the my own project. As basis I am using Ux_Device_CDC_ACM Example provided by ST as reference.

It was discovered that Ux_Device_CDC_ACM example would not work properly after MxCube project regeneration -- it goes to the HardFault_Handler() at some point (not defined currently at which point)

The investigation showed that the issue is connected with the Optimization level (MxCube updated STM32CubeIDE project files) just only for the one single source file: "stm32n6xx_hal_rcc_ex.c". If optimization level is set to "-O0" for the mentioned file -- HardFault_Handler() is observed. By changing it to the "-O3" -- the application works successfully.

Could you please explain this "hidden" dependency, and what is the reason of this?

4 replies

Pavel A.
April 24, 2026

>  it goes to the HardFault_Handler() at some point (not defined currently at which point)

Can you tell more how to reproduce this? What does the program do when the HardFault occurs? Do you have the register values? Change in the optimization level in one .c file can just move code & data of other modules to other addresses, it may not be the root cause at all.

bureau
bureauAuthor
Associate II
April 24, 2026

The simplest way to reproduce it:

  1. Open (import) the Ux_Device_CDC_ACM example into the STM32CubeIDE
    The example project could be found in  the folder:
    STM32Cube_FW_N6_V1.3.0\Projects\NUCLEO-N657X0-Q\Applications\USBX\Ux_Device_CDC_ACM
  2. In the project Explorer find the file: stm32n6xx_hal_rcc_ex.c
    Drivers/STM32N6xx_HAL_Driver/stm32n6xx_hal_rcc_ex.c
  3. Press Properties on the file
  4. Go to the C/C++ Build --> Settings -- > Optimization
  5. Observe that it was selected O3 (when for the other files it is set O0)
  6. Change Optimization level for the stm32n6xx_hal_rcc_ex.c to O0
  7. Compile --> Debug/Run

 

ST Technical Moderator
April 27, 2026

Hello @bureau 

Since -O0 generally produces larger stack frames than -O3, the HardFault may be caused by an insufficient stack allocation rather than by the RCC source file itself. For this reason, we recommend increasing the stack size as a first diagnostic step.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Andrew Neil
Super User
April 27, 2026
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.