Skip to main content
Associate II
August 22, 2026
Solved

Hard Fault in TCP Echo Server (Ethernet)

Hi all , 

Im facing a issue in TCP/IP - Ethernet using LWIP on STM32H723ZGT6 [NUCLEO - H723ZG] , that i gave completed ethernet configuration , ping is good , wrote a tcp_echoserver and modified with my desired outputs , everything was a woking upto a certain level, and i cant RX and Tx and fall into hard fault (Added a Video of the output). I'll add the code file as a zip. 

Kindly help me to resolve ii.

Thank You!!!.....

Associate II
August 22, 2026

Thank you for all your reply, 

I have resolved it , 2hrs ago forgot to mention in the community, the issue was i have mapped my LWIP Rx pool at 0x30000400 at 16KB (approximately ends at 0x30004400) and set my lwip heap at 0x30004000 so both of them are overlapped , so only i got hardfault , finnally found and resolved it by placing the heap  @ 0x30005000. 

 

3 replies

Gokul_Sarvanakumar_60AuthorBest answer
Associate II
August 22, 2026

Thank you for all your reply, 

I have resolved it , 2hrs ago forgot to mention in the community, the issue was i have mapped my LWIP Rx pool at 0x30000400 at 16KB (approximately ends at 0x30004400) and set my lwip heap at 0x30004000 so both of them are overlapped , so only i got hardfault , finnally found and resolved it by placing the heap  @ 0x30005000. 

 

Andrew Neil
Super User
August 22, 2026

Debugging Cortex-M Hard Faults

LwIP debug & diagnostic options.

 


@Gokul_Sarvanakumar_60  wrote:

everything was a woking upto a certain level, and i cant RX and Tx and fall into hard fault...


As  @Uwe Bonnes  said, go back to the last working version; examine carefully what you changed.

Use the above-mentioned LwIP debug & diagnostic options to compare & contrast what happens in the working & non-working cases ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Uwe Bonnes
Chief
August 22, 2026

Hopefully you developped und revison control, e.g. with GIT. Then you can bisect to find the bad commit...