Skip to main content
MHoop.1
Senior
Mar 7, 2023 5:29 PM UTC
Solved

Hard Fault in Azure RTOS NetX Duo NUCLEO-F7 with newly upgraded CubeIDE V1.12

Once again.....trying to implement an Azure RTOS NX TCP Server application on the F7 Nucleo board (since H7 processors will not be available any time soon). I ran into a hard fault at the HAL_GetTick instruction below:

 /*-------------------------------- PLL Configuration -----------------------*/
 /* Check the parameters */
 assert_param(IS_RCC_PLL(RCC_OscInitStruct->PLL.PLLState));
 if ((RCC_OscInitStruct->PLL.PLLState) != RCC_PLL_NONE)
 {
 /* Check if the PLL is used as system clock or not */
 if(__HAL_RCC_GET_SYSCLK_SOURCE() != RCC_CFGR_SWS_PLL)
 {
 if((RCC_OscInitStruct->PLL.PLLState) == RCC_PLL_ON)
 {
 /* Check the parameters */
 assert_param(IS_RCC_PLLSOURCE(RCC_OscInitStruct->PLL.PLLSource));
 assert_param(IS_RCC_PLLM_VALUE(RCC_OscInitStruct->PLL.PLLM));
 assert_param(IS_RCC_PLLN_VALUE(RCC_OscInitStruct->PLL.PLLN));
 assert_param(IS_RCC_PLLP_VALUE(RCC_OscInitStruct->PLL.PLLP));
 assert_param(IS_RCC_PLLQ_VALUE(RCC_OscInitStruct->PLL.PLLQ));
 
 /* Disable the main PLL. */
 __HAL_RCC_PLL_DISABLE();
 
 /* Get Start Tick */
 tickstart = HAL_GetTick(); <<<<<<<< Hard Fault >>>>>>

This is using a newly updated CubeIDE (V1.12) and imported example code.

Any sage advice?

thx

Mikeh

This topic has been closed for replies.
MHoop.1
MHoop.1Best answer
Senior
Mar 7, 2023 6:07 PM UTC

Sorry....operator error. Plugged in the wrong Nucleo board. With the correct Nucleo board I am able to get the basic example running with no problem.

1 reply

MHoop.1
MHoop.1AuthorBest answer
Senior
Mar 7, 2023 6:07 PM UTC

Sorry....operator error. Plugged in the wrong Nucleo board. With the correct Nucleo board I am able to get the basic example running with no problem.