Skip to main content
Associate II
Jan 29, 2026 6:30 AM UTC
Question

Hard Fault During USBX Host MSC Example Execution on STM32H573 DK

Hello Everyone,

I hope this message finds you well. I am currently developing a USB Host application using the STM32H573I-DK and have encountered a persistent Hard Fault issue that I would like to seek your expertise on.


[Environment Information]

Target: STM32H573I-DK

Example: USBPD_SRC_UX_Host_MSC 

Stack: Azure RTOS (ThreadX, USBX)

[Detailed Symptom]

Hosung_0-1769668005924.png

A hard fault occurs during initialization or while driving the process thread (msc_process_thread_entry) when connecting a USB MSC device. Debugging revealed abnormal memory access occurring during execution of the _ux_utility_memory_copy function.


[Inquiry]
When implementing USBX Host in this example and the STM32H5 environment, we seek broad advice on potential causes that could trigger memory copy and access errors.

Example Stability: Are there any known issues or patch histories related to USBX memory management or stack configuration in the currently deployed USBPD_SRC_UX_Host_MSC example?

H5 Architecture Characteristics: Are there scenarios where the STM32H573's I-Cache/D-Cache policies, MPU settings, or constraints on the Bus Matrix could impact the behavior of USBX utility functions (e.g., `_ux_utility_memory_copy`)?

Memory Layout and Alignment: Where might a hard fault occur if section placement (RAM region division) or alignment requirements for the USBX system memory pool or MSC dedicated buffer are missing?

Debugging Guide: Please advise if there are any additional registers or logs to check to trace the root cause of _ux_utility_memory_copy referencing an invalid address (e.g., race conditions, pointer corruption, etc.).

Best Regards, Hosung Han

1 reply

ST Technical Moderator
Jan 29, 2026 5:36 PM UTC

Hello @Hosung 

Are you using latest version of the application?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL