Skip to main content
IKayk.1
Associate
Jun 8, 2021 2:16 PM UTC
Question

HAL_UART_Transmit_DMA transmits data with delay

Hi,

I have written an STM32 program that transmits data using HAL_UART_Transmit_DMA .

However, for some reason, the first time I call this HAL function, Rx line only outputs 0s.

The second message I'm sending actually sends the first message,

The third message sends the second, and so on.

I have verified with debug that each call to the HAL function has the correct message in the buffer parameter, and I have verified with scope (the scope I used can interpret the outgoing message) that every message that goes out of the Rx pin is the previous one.

this is the code that is called in a loop, please note that I'm always getting HAL_OK as a return value:

if( m_configuration.huart->gState == HAL_UART_STATE_READY ) {
 
		if( HAL_OK == HAL_UART_Transmit_DMA( m_configuration.huart, reinterpret_cast< U08 * >( pData ), static_cast< uint16_t >( length ))) {
 
			amount = length ;
		}
	}
	else{
 
		amount = itsTUtilityCircularBufferTx.putElements( reinterpret_cast< U08 * >( pData ), length ) ;
	}

Is this a known issue?

This topic has been closed for replies.

2 replies

TDK
Jun 8, 2021 2:27 PM UTC

Sounds like a mismanaged cache issue. What STM32?

Although if the behavior is super regular, sounds more like a bug somewhere in the code or in your interpretation of it.

"If you feel a post has answered your question, please click ""Accept as Solution""."
IKayk.1
IKayk.1Author
Associate
Jun 8, 2021 2:36 PM UTC

Sorry, I forgot to mention, I use STM32H743ZI2 (Nucleo Board EVB).

Perhaps I should have mentioned that currently I'm sending messages in, and using a counter sending responses to these messages.

I receive all the messages in the correct order, verified by debugging the code.

However, when sending out my response, this issue causes a mismatch in my flow because the first message gets a bunch of 0s as answer, the second message gets the first message response, etc.