Skip to main content
Associate II
June 30, 2026
Question

HAL Suggestion: Allow EXTI and AF on same GPIO input

Some applications have the need to use an external interrupt from an GPIO input that is already configured as alternate function. My use case is to use EXTI on a rising edge of SPI_NSS input to detect a terminated SPI transfer on a slave.

So I need the combination of MODE_AF and EXTI_IT when configuring the GPIO input pin. Unfortunately, HAL does not support this and asserts on IS_GPIO_MODE(__MODE__) for this combination.

However, STM32 MCUs usually support this combination, so it makes sense to support this in HAL.

To allow this, I added some definitions in stm32g4xx_hal_gpio.h:

#define  GPIO_MODE_AF_IT_RISING                    (MODE_AF | EXTI_IT | TRIGGER_RISING)                     /*!< Alternate Function with External Interrupt Mode with Rising edge trigger detection          */ 
#define GPIO_MODE_AF_IT_FALLING (MODE_AF | EXTI_IT | TRIGGER_FALLING) /*!< Alternate Function with External Interrupt Mode with Falling edge trigger detection */
#define GPIO_MODE_AF_IT_RISING_FALLING (MODE_AF | EXTI_IT | TRIGGER_RISING | TRIGGER_FALLING) /*!< Alternate Function with External Interrupt Mode with Rising/Falling edge trigger detection */

and updated the 

#define IS_GPIO_MODE(__MODE__)

macro accordingly. No change in stm32g4xx_hal_gpio.c needed.

I suggest to add this to the STM32 HAL drivers of the MCUs that support this combination.

Regards, Norbert

 

1 reply

ST Technical Moderator
June 30, 2026

 

Hello ​@unterberg_rtb 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: CDM0063933 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om