Skip to main content
Visitor II
Mar 7, 2025 3:24 PM UTC
Question

HAL_PCDEx_PMAConfig Calculation help for Stream of YUY2 Image format.

Hello! 

I am working on Implementing a Uncompressed YUV2 Stream through the Windows Camera Application with an STM32H5 Series Board. I am looking for an example of these values, the HAL_PCDEx_PMAConfig Values, as these are what establish the USB payload buffer to send my images through a stream2.h file found in this project (https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/NUCLEO-H723ZG/Applications/USBX/Ux_Device_Video/Stream) . The H5 doesn't support USB-OTG, so I have been trying to find an example of a project that is a USBX Video that uses USB FS functionality. (The linked project uses USB-OTG so instead it uses HAL_PCDEx_SetRxFiFo/SetTxFifo to establish a payload)

 

These values worked with the stream1.h file from that same project linked above. However I am unable to change these values for a YUV2 stream to successfully stream. 

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x00, PCD_SNG_BUF, 0x10);

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x80, PCD_SNG_BUF, 0x50);

HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS,USBD_VIDEO_EPIN_ADDR , PCD_DBL_BUF, 0x01900090);

 

Any guidance? 

 

This topic has been closed for replies.

1 reply

ST Technical Moderator
Apr 29, 2025 10:45 AM UTC

Hi @treepreeyuh 

Have you tried to generate code using CubeMX?

FBL_0-1745922413177.png

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL