HAL_I2S_TransmitDMA in circular mode (STM32H503) doesn't run continuously
- June 8, 2025
- 8 replies
- 829 views
I have set up a DMA on an I2S device with an STM32H503CBU6. The idea is, that the DMA runs continuously on a single bufferaddress (one word, containing the left and right channels for the external I2S-DAC). When the DMA transfer of that 1 word is complete it should start over again by itself.
At present the goal is not achieved with the following setup:
uint16_t ram_loc[2] = {0,0};
int main(void)
{
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_GPDMA1_Init();
MX_ICACHE_Init();
MX_I2C1_Init();
MX_I2S2_Init();
MX_TIM1_Init();
HAL_I2S_Transmit_DMA(&hi2s2, ram_loc,1); // since circular is configured,
// am I right that the DMA keeps alive itself?
/* USER CODE END 2 */
/* Infinite loop */
while (1)
{
// for testing, increment ram_loc (L+R) by one every 10ms
// which should produce a (sawtooth) ramp.
//
HAL_Delay(10);
ram_loc[0]++,ram_loc[1]++;
if(ram_loc[0] == 65535)
ram_loc[0]=ram_loc[1]=0;
}
}
Some things I'm not sure about: how is the DMA data organized. Since it is an I2S audio stream with L+R signals, I assume they are two words of 16bits, sent in one 32bit DMA chunk. Or is it 32bit data in a 32bit frame? BTW, what does "frame" actually stand for?
What is the "Port 0" that appears, when I choose "circular" mode in the DMA channel 4 setup?
I2S2_WS - PA3
I2S2_CK - PA5
I2S2_SDO - PB1I don't see any data on PB1. Timing is there (48KHz on PA5, WS on PA3).