Skip to main content
uahma
Associate
November 14, 2018
Question

HAL I2S timeout error

  • November 14, 2018
  • 2 replies
  • 910 views

HAL I2S timeout error, look at my code below, i had it working one day and now it never works, the HAL_I2S_Receive function is only called once and then I run into HAL_StatusTypeDef being stuck in HAL_TIMEOUT.

while (1)
 
 {
 
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 
 HAL_StatusTypeDef result = HAL_I2S_Receive(&hi2s1, (uint16_t*)I2S_RX_BUFFER, 24, 100);
 
 HAL_Delay(500);
 
 if(result == HAL_OK){
 
 volatile int32_t data_full = (int32_t) I2S_RX_BUFFER[0] << 16 | I2S_RX_BUFFER[1];
 
 volatile int16_t data_short = (int16_t) I2S_RX_BUFFER[0];
 
 
 volatile uint32_t counter = 2;
 
 while(counter--);
 
 HAL_Delay(500);
 
 }
 
 }

I did make use of __HAL_DBGMCU_UNFREEZE_IWDG() before my HAL_Init(); command but still it does not work. I swear it worked once and i was able to get different sensor data while debugging with GDB server but not anymore and this is driving me crazy.

my code is stuck in result = HAL_TIMEOUT .....

This topic has been closed for replies.

2 replies

Amel NASRI
ST Technical Moderator
November 15, 2018

Hello,

Please:

  1. use a meaningful title/summary for your question
  2. use "Code Snippet" icon to insert code
  3. precise the device you are using

I edited your question to make these updates. This way, your question will be easier to understand, and you will have more chance to get an answer.

Thanks for your understanding.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
uahma
uahmaAuthor
Associate
November 15, 2018

Thanks Amel.