Question
HAL_I2C_Master_Transmit & HAL_I2C_Master Receive never return with HAL_OK using I2C2 Using cube 5.0 generated init's and using the F4_V1.24.0 library.
I2C2 is PB11,PB10 are connected to an AT24CM01 I2C eeprom. I get a few writes to the DR then the hal decided that the device is busy and all other calls fail because the device is busy. My writes and reads are trying to to do 240 bytes, not a very large packet. We are running the device slow, 8mhz crystal, 32 mhz internal bus to conserve power. I have verified that the hal sets up the pins to open drain alternate function i2c.