Skip to main content
Associate II
Mar 26, 2025 12:15 PM UTC
Question

HAL_GPIO_EXTI_Callback - using rising edge and falling edge

I use it to see if R S T is present in 3-phase systems with F072 c8t6 processor. I have defined only R pin as interrupt, the other two are defined as input. When I write the code as below, I cannot check the status of R. I guess it is because of the version or the processor I cannot use HAL_GPIO_EXTI_Rising_Callback

CODE:

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)

{



 sPhase_t *rstPhase = &taskPeripheralUnits.phase;

 if(GPIO_Pin == ioR_Pin)

 {

 if (HAL_GPIO_ReadPin(ioR_GPIO_Port, ioR_Pin))

 {

 rstPhase->ucRawPhaseData[ZERO][rstFACTOR_R_PHASE] = ACTIVE;

 rstPhase->ucRawPhaseData[ZERO][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioS_GPIO_Port, ioS_Pin);

 rstPhase->ucRawPhaseData[ZERO][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioT_GPIO_Port, ioT_Pin);

 }

 else

 {

 rstPhase->ucRawPhaseData[1u][rstFACTOR_R_PHASE] = PASSIVE;

 stPhase->ucRawPhaseData[1u][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioS_GPIO_Port, ioS_Pin);

 rstPhase->ucRawPhaseData[1u][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioT_GPIO_Port, ioT_Pin);

 }

 }

}

 

This topic has been closed for replies.

6 replies

KnarfB
Super User
Mar 26, 2025 12:28 PM UTC

The hardware is capable to select raising or falling external interrupt edge or both. This is reflected in STM32CubeMX as well.  

> I cannot check the status of R

You are reading the pin level with HAL_GPIO_ReadPin.

So, what unexpected behaviour exactly are you observing? 

hth

KnarF

Associate II
Mar 26, 2025 12:34 PM UTC

 I check whether there are 3 phases according to the states of the RS and T pins, but here the value of R always comes as 0 1 0 1. In my code, when R is 0, I write a voltage error, but even though R = 0, the error is not entered.

KnarfB
Super User
Mar 26, 2025 4:15 PM UTC

> the value of R always comes as 0 1 0 1

That's what I would expect from a periodic signal.

KnarfB

mƎALLEm
ST Technical Moderator
Mar 26, 2025 12:29 PM UTC

Hello,

The question is not clear. Could you please elaborate/reword?

Regarding HAL_GPIO_EXTI_Rising_Callback() it's not available on STM32F0 CubeHAL. HAL_GPIO_EXTI_Rising_Callback() is available on STM32F0 CubeHAL like what you shared in your post.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate II
Mar 27, 2025 8:12 AM UTC
What I mean is this I have a code that controls 3 phases on the stm32u073 processor. There are HAL_GPIO_EXTI_Rising_Callback and HAL_GPIO_EXTI_Falling_Callback functions on that processor and I posted the code as in the example and it works properly. However, I only changed HAL_GPIO_EXTI_Callback on the stm32F072C8T6 and it does not work. Could there be a problem due to these functions?

/*Code with U073*/
void HAL_GPIO_EXTI_Falling_Callback(uint16_t GPIO_Pin)
{
 sPhase_t *rstPhase = &taskPeripheralUnits.phase;
 if (GPIO_Pin == ioINPEXT_R_Pin)
 {
 rstPhase->ucRawPhaseData[1u][rstFACTOR_R_PHASE] = PASSIVE;
 rstPhase->ucRawPhaseData[1u][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioINP_S_GPIO_Port, ioINP_S_Pin);
 rstPhase->ucRawPhaseData[1u][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioINP_T_GPIO_Port, ioINP_T_Pin);
 }
}
/*---------------------------------------------------------------------------------------------------------------------------*/
void HAL_GPIO_EXTI_Rising_Callback(uint16_t GPIO_Pin)
{
 sPhase_t *rstPhase = &taskPeripheralUnits.phase;
 if (GPIO_Pin == ioINPEXT_R_Pin)
 {
 rstPhase->ucRawPhaseData[ZERO][rstFACTOR_R_PHASE] = ACTIVE;
 rstPhase->ucRawPhaseData[ZERO][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioINP_S_GPIO_Port, ioINP_S_Pin);
 rstPhase->ucRawPhaseData[ZERO][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioINP_T_GPIO_Port, ioINP_T_Pin);
 }
}
/*---------------------------------------------------------------------------------------------------------------------------*/
static void prvRstPhaseExistanceCtrl(void)
{
 sPhase_t *rstPhase = &taskPeripheralUnits.phase;
 static TickType_t xTickTimer;
 uint8_t Rdetected, Sdetected, Tdetected;
 uint8_t *ucPhases[rstPHASE_COUNT_TOTAL] = {&Rdetected, &Sdetected, &Tdetected};

 for (int Idx = ZERO; Idx < rstPHASE_COUNT_TOTAL; Idx++)
 {
 if (!(rstPhase->ucRawPhaseData[0][Idx] & rstPhase->ucRawPhaseData[1][Idx]) )
 {
 *(ucPhases[Idx]) = ACTIVE;
 }
 else
 {
 *(ucPhases[Idx]) = PASSIVE;
 }
 }

 if((Rdetected & Sdetected & Tdetected) == ACTIVE)
 {
 xTickTimer = xTaskCurrentTick;
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_DETECTED;
 }
 else
 {
 taskPeripheralUnits.phase.sequenceStatus.ucSequence = rstPHASE_SEQUENCE_WRONG;

 if (xTaskCurrentTick - xTickTimer > timeDELAY_RST_CONTROL)
 {
 if((Rdetected & Sdetected) == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_RS_DETECTED;
 }
 else if((Sdetected & Tdetected) == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ST_DETECTED;
 }
 else if((Tdetected & Rdetected) == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_RT_DETECTED;
 }
 else if(Rdetected == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_R_DETECTED;
 }
 else if(Sdetected == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_S_DETECTED;
 }
 else if(Tdetected == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_T_DETECTED;
 }
 else /* None of them Active */
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_NOT_DETECTED;
 }
 }
 else
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_DETECTED;
 }
 }
}

/* Code with F072 */ 

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{

 sPhase_t *rstPhase = &taskPeripheralUnits.phase;
 if(GPIO_Pin == ioR_Pin)
 {
 if (HAL_GPIO_ReadPin(ioR_GPIO_Port, ioR_Pin) == GPIO_PIN_RESET)
 {
 rstPhase->ucRawPhaseData[ZERO][rstFACTOR_R_PHASE] = ACTIVE;
 rstPhase->ucRawPhaseData[ZERO][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioS_GPIO_Port, ioS_Pin);
 rstPhase->ucRawPhaseData[ZERO][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioT_GPIO_Port, ioT_Pin);
 }
 else
 {
 rstPhase->ucRawPhaseData[1u][rstFACTOR_R_PHASE] = PASSIVE;
 rstPhase->ucRawPhaseData[1u][rstFACTOR_S_PHASE] = HAL_GPIO_ReadPin(ioS_GPIO_Port, ioS_Pin);
 rstPhase->ucRawPhaseData[1u][rstFACTOR_T_PHASE] = HAL_GPIO_ReadPin(ioT_GPIO_Port, ioT_Pin);
 }

 }
}
/*---------------------------------------------------------------------------------------------------------------------------*/
static void prvRstPhaseExistanceCtrl(void)
{
 sPhase_t *rstPhase = &taskPeripheralUnits.phase;
 static TickType_t xTickTimer;
 uint8_t Rdetected, Sdetected, Tdetected;
 uint8_t *ucPhases[rstPHASE_COUNT_TOTAL] = {&Rdetected, &Sdetected, &Tdetected};
 for (int Idx = ZERO; Idx < rstPHASE_COUNT_TOTAL; Idx++)
 {
 if (!(rstPhase->ucRawPhaseData[0][Idx] & rstPhase->ucRawPhaseData[1][Idx]) )
 {
 *(ucPhases[Idx]) = ACTIVE;
 }
 else
 {
 *(ucPhases[Idx]) = PASSIVE;
 }
 }

 if((Rdetected & Sdetected & Tdetected) == ACTIVE)
 {
 xTickTimer = xTaskCurrentTick;
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_DETECTED;
 vSciPrintf((uint8_t *) "1\n");
 }
 else
 {
 taskPeripheralUnits.phase.sequenceStatus.ucSequence = rstPHASE_SEQUENCE_WRONG;

 if (xTaskCurrentTick - xTickTimer > timeDELAY_RST_CONTROL)
 {
 if((Rdetected & Sdetected) == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_RS_DETECTED;
 vSciPrintf((uint8_t *) "2\n");
 }
 else if((Sdetected & Tdetected) == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ST_DETECTED;
 vSciPrintf((uint8_t *) "3\n");
 }
 else if((Tdetected & Rdetected) == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_RT_DETECTED;
 vSciPrintf((uint8_t *) "4\n");
 }
 else if(Rdetected == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_R_DETECTED;
 vSciPrintf((uint8_t *) "5\n");
 }
 else if(Sdetected == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_S_DETECTED;
 vSciPrintf((uint8_t *) "6\n");
 }
 else if(Tdetected == ACTIVE)
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_T_DETECTED;
 vSciPrintf((uint8_t *) "7\n");
 }
 else /* None of them Active */
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_NOT_DETECTED;
 vSciPrintf((uint8_t *) "8\n");
 }
 }
 else
 {
 rstPhase->sequenceStatus.ucStatus = rstPHASE_STATUS_ALL_DETECTED;
 }
 }
}
mƎALLEm
ST Technical Moderator
Mar 27, 2025 8:14 AM UTC

Hello,

Please use </> to share your code. I'm editing your post.

You can refer to this link on how to do it.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.