Skip to main content
keebler411
Associate II
Jan 23, 2019 8:53 PM UTC
Question

HAL_GetUID functions do not seem to work

The HAL_GetUID functions return the same value on different chips of the same series. I am using an STM32L0 series chip. This is my code:

uint32_t serialw0 = HAL_GetUIDw0();
uint32_t serialw1 = HAL_GetUIDw1();
uint32_t serialw2 = HAL_GetUIDw2();

Which returns these sames values on every chip:

205994032, 926167089, 17

Searching through the generated files this is code for the above functions:

#define UID_BASE (0x1FF80050UL) /*!< Unique device ID register base address */
 
uint32_t HAL_GetUIDw0(void)
{
 return(READ_REG(*((uint32_t *)UID_BASE)));
}
 
uint32_t HAL_GetUIDw1(void)
{
 return(READ_REG(*((uint32_t *)(UID_BASE + 4U))));
}
 
uint32_t HAL_GetUIDw2(void)
{
 return(READ_REG(*((uint32_t *)(UID_BASE + 8U))));
}
 

Now if write my own macro:

#define STM32_UUID ((uint32_t *)(0x1FF80050))
uint32_t serialw0 = *(STM32_UUID);
uint32_t serialw1 = *(STM32_UUID+4U);
uint32_t serialw2 = *(STM32_UUID+8U);

I get unique values for each chip but I don't think this is correct either:

205994032, 3432448017, 0

In fact its only word1 that seems to be unique which I suppose could be correct.

This topic has been closed for replies.

4 replies

Marcelo Barros
Associate III
Feb 13, 2019 7:32 AM UTC

I had a problem related to HAL_GetUIDw2() when using STM32L0x1/STM32L0x2. Checkingvthe user manual, the third ID word is not located at UID_BASE+8. Instead, it is at position UID_BASE+20. So, HAL_GetUIDw2() seems to point to the wrong position. The first two words are related to lot number and waffer number and only int the third word we have a factory programmed unique ID for this lot.

I suggest you check you user manual at section "Unique device ID registers".

ST Technical Moderator
Feb 13, 2019 10:57 AM UTC

Hello,

You are right. After check, we confirm that 0x14 is the correct offset for HAL_GetUIDw2 (as mentioned in the STM32L0 Reference Manual).

I raised this issue internally to developer team for fix and correct stm32L0xx_hal.c file (line 414)

// return(READ_REG(*((uint32_t *)(UID_BASE + 8U))));

So, this line should be:

return(READ_REG(*((uint32_t *)(UID_BASE + 20U))));

Thank you for highlighting this issue.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
keebler411
Associate II
Feb 15, 2019 8:47 PM UTC

Thanks for the confirmation. I'm just learning this platform and problems like this don't help, but I understand mistakes happen. Not like I haven't done similar either ;)

Associate II
May 7, 2024 5:21 PM UTC

Do other chip series have a similar offset problem?  I am using STM32U family.

In my framework code, it uses BASE+0, BASE+4, BASE+8