HAL_GetTick() function of STM32F0 driver is blocking SPI interrupts
Hello,
I have a problem with ''HAL_GetTick()'' that is blocking the SPI interrupt. In my program, I use the ''HAL_SPI_Transmit_IT'' function from STM32F0 HAL driver library to initiate a SPI transmission. After a while, a SPI interrupt occurs and the following functions are called:
In the last called function (''HAL_StatusTypeDef SPI_WaitFifoStateUntilTimeout'' function of ''STM32F0xx_HAL_Driver\Src\stm32f0xx_hal_spi.c'' file), the following instruction is blocking my program:
if
((Timeout == 0) || ((HAL_GetTick()-tickstart) >= Timeout))
The tick value is always the same (217) and the program can’t run out of this function until this condition is true.
First, I put a breakpoint in function '' GetTick()'' (from '' STM32F0xx_HAL_Driver\Src\stm32f0xx_hal.c'' file but nothing happened: the function was never called.
In the
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00122pdf
(STM32F0 driver datasheet), I saw the following note for the ''HAL_InitTick'' function:
Care must be taken if HAL_Delay() is called from a peripheral ISR process, The the SysTick interrupt must have higher priority (numerically lower) than the peripheral interrupt. Otherwise the caller ISR process will be blocked.
Following this note, I configured all the other interrupts with a lower priority in my STM32CubeMx project:

Unfortunately, this didn’t change anything.
Does someone have another idea to solve this issue?
Note: the firmware package library I’m currently using is version 1.3.0.
#hal_gettick()-blocking-interrupt