Skip to main content
Christoph Eschenbach
Associate III
July 16, 2018
Question

HAL_ETH Drivers, ReadPHYRegister problem

  • July 16, 2018
  • 0 replies
  • 832 views
Posted on July 16, 2018 at 10:15

Hello there,

I have some problem understanding the ReadPHYRegister-Function from the stm32f4xx_hal_eth.c.

I am using the Stm32f429 and a LAN8742A. On a nucleo board and on a custom board.

Primary with the parameter uint16_t PHYReg.

So in the datasheet the Register indexes are number 0-31 with skipping some numbers. So i expected to use those indexes for the param PHYReg. But I am not sure if i read the registers with the correct index.

The 'Interrupt Source Flag Register' has Index 29 (0x1D) and the 'Interrupt Mask Register' 30(0x1E)

In stm32f4xx_hal_conf.h is the definition for the ' Interrupt Source Flag register offset'

&sharpdefine PHY_ISFR   ((uint16_t)0x000Bu)

and more irritating

/* Phy link down interrupt offsett */

&sharpdefine PHY_ISFR_INT4   ((uint16_t)0x000Bu)

which is described in the data sheets as Bit 4( 0x04). For this i can explain when you count from the msb but not for the PHY_ISFR.

On the nucleo board i have no problems with the cubemx drivers all interrupts get detected. On my custom board it was working once unfortunatley now the interrupts dont get detected. So i need to debug the lan8742A and reading the registers correct is mandatory for this.

#external-phy #hal_eth #stm32f429 #ethernetif #lan8742a
This topic has been closed for replies.