Skip to main content
Mohammad A
Senior
March 19, 2018
Question

HAL Drivers User Manual Eclipse Help

Posted on March 19, 2018 at 17:45

I wanted to ask if it would be possible for ST to make HAL drivers user manual available for eclipse help. As HAL user manual is written in doxygen format, this is easy to generate eclipse specific help files.

This is a part of Doxyfile configuration which is used to generate doxygen documents:

♯ If the GENERATE_ECLIPSEHELP tag is set to YES, additional index files will be

♯ generated, together with the HTML files, they form an Eclipse help plugin. To

♯ install this plugin and make it available under the help contents menu in

♯ Eclipse, the contents of the directory containing the HTML and XML files needs

♯ to be copied into the plugins directory of eclipse. The name of the directory

♯ within the plugins directory should be the same as the ECLIPSE_DOC_ID value.

♯ After copying Eclipse needs to be restarted before the help appears.

These user manual files are only available under CHM format at the moment.

#hal #document #user-manual
This topic has been closed for replies.

3 replies

Mohammad A
Senior
March 20, 2018
Posted on March 20, 2018 at 16:46

Why not?

Tesla DeLorean
Guru
March 20, 2018
Posted on March 20, 2018 at 16:53

Couldn't you run the processing tools against the library sources and get it out in a form that suits you?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Mohammad A
Senior
March 20, 2018
Posted on March 20, 2018 at 17:10

No.

It needs other descriptor files which are not available.

I tried, but didn't work.