Skip to main content
MSipo
Senior II
December 15, 2020
Question

HAL Bug in stm32l1xx_hal.c?

I'm using FirmwarePackage=STM32Cube FW_L1 V1.10.1

I'm looking at these functions in stm32l1xx_hal.c:

/**
 * @brief Return the first word of the unique device identifier (UID based on 96 bits)
 * @retval Device identifier 31:0 bits
 */
uint32_t HAL_GetUIDw0(void)
{
 return(READ_REG(*((uint32_t *)UID_BASE)));
}
 
/**
 * @brief Return the second word of the unique device identifier (UID based on 96 bits)
 * @retval Device identifier 63:32 bits
 */
uint32_t HAL_GetUIDw1(void)
{
 return(READ_REG(*((uint32_t *)(UID_BASE + 0x4U))));
}
 
/**
 * @brief Return the third word of the unique device identifier (UID based on 96 bits)
 * @retval Device identifier 95:64 bits
 */
uint32_t HAL_GetUIDw2(void)
{
 return(READ_REG(*((uint32_t *)(UID_BASE + 0x14U))));
}

They do not use a volatile pointer. Shouldn't they? Could a compiler optimize this in a bad way?

I would write them as:

return *((__IO uint32_t *)UID_BASE);

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
December 15, 2020

Why would it need to be volatile? The content doesn't change between reads.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MSipo
MSipoAuthor
Senior II
December 15, 2020

But the IDCODE register is defined volatile and that doesn't either change?

/** 
 * @brief Debug MCU
 */
 
typedef struct
{
 __IO uint32_t IDCODE; /*!< MCU device ID code, Address offset: 0x00 */
 __IO uint32_t CR; /*!< Debug MCU configuration register, Address offset: 0x04 */
 __IO uint32_t APB1FZ; /*!< Debug MCU APB1 freeze register, Address offset: 0x08 */
 __IO uint32_t APB2FZ; /*!< Debug MCU APB2 freeze register, Address offset: 0x0C */
}DBGMCU_TypeDef;

Tesla DeLorean
Guru
December 15, 2020

And do those actually need to be volatile either? I think you're working this problem in the wrong direction.

A bug would be a situation where something changed outside of program control/flow and wasn't marked as volatile.

The blanket __IO in the structures avoids a lot of register level evaluation and maintenance on the library maintainers part, some of whom might not have a particularly strong understanding of the exact HW interactions at a bit/register level.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..