Skip to main content
yuming
Associate
October 21, 2019
Question

HAL_ADC_Start_DMA example, always get value 0

  • October 21, 2019
  • 2 replies
  • 3573 views

hi guys, i'm stm freshman, I am trying to read the adc value by using the adc example of stm32f4, I added bold code to get uhADCxConvertedValue value, but uhADCxConvertedValue value always get 0 Whether I connect adc pin to grounded or vcc.

the led4 and led3​ is bright.

example:

STM32 DISCO board's LEDs can be used to monitor the transfer status:

 - LED4 is ON when the conversion is complete.

 - LED5 is ON when there are an error in initialization.

​

code:

int main(void)

{

 ADC_ChannelConfTypeDef sConfig;

  

 /* STM32F4xx HAL library initialization:

    - Configure the Flash prefetch, instruction and Data caches

    - Configure the Systick to generate an interrupt each 1 msec

    - Set NVIC Group Priority to 4

    - Global MSP (MCU Support Package) initialization

   */

 HAL_Init();

  

 /* Configure the system clock to 144 MHz */

 SystemClock_Config();

  

 /* Configure LED4 and LED5 */

 BSP_LED_Init(LED4);

 BSP_LED_Init(LED5);

BSP_LED_Init(LED3);

 BSP_LED_Init(LED6);

  

 /*##-1- Configure the ADC peripheral #######################################*/

 AdcHandle.Instance = ADCx;

  

 AdcHandle.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV2;

 AdcHandle.Init.Resolution = ADC_RESOLUTION_12B;

 AdcHandle.Init.ScanConvMode = DISABLE;

 AdcHandle.Init.ContinuousConvMode = ENABLE;

 AdcHandle.Init.DiscontinuousConvMode = DISABLE;

 AdcHandle.Init.NbrOfDiscConversion = 0;

 AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

 AdcHandle.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T1_CC1;

 AdcHandle.Init.DataAlign = ADC_DATAALIGN_RIGHT;

 AdcHandle.Init.NbrOfConversion = 1;

 AdcHandle.Init.DMAContinuousRequests = ENABLE;

 AdcHandle.Init.EOCSelection = DISABLE;

    

 if(HAL_ADC_Init(&AdcHandle) != HAL_OK)

 {

  /* Initialization Error */

  Error_Handler(); 

 }

  

 /*##-2- Configure ADC regular channel ######################################*/

 /* Note: Considering IT occurring after each number of size of       */

 /*    "uhADCxConvertedValue" ADC conversions (IT by DMA end       */

 /*    of transfer), select sampling time and ADC clock with sufficient  */

 /*    duration to not create an overhead situation in IRQHandler.    */  

 sConfig.Channel = ADCx_CHANNEL;

 sConfig.Rank = 1;

 sConfig.SamplingTime = ADC_SAMPLETIME_28CYCLES;

 sConfig.Offset = 0;

  

 if(HAL_ADC_ConfigChannel(&AdcHandle, &sConfig) != HAL_OK)

 {

  /* Channel Configuration Error */

  Error_Handler(); 

 }

​

 /*##-3- Start the conversion process and enable interrupt ##################*/

 /* Note: Considering IT occurring after each number of ADC conversions   */

 /*    (IT by DMA end of transfer), select sampling time and ADC clock  */

 /*    with sufficient duration to not create an overhead situation in  */

 /*    IRQHandler. */ 

 if(HAL_ADC_Start_DMA(&AdcHandle, (uint32_t*)&uhADCxConvertedValue, 1) != HAL_OK)

 {

  /* Start Conversation Error */

  Error_Handler(); 

 }

​

 uint32_t Value1 = 0;

Value1=uhADCxConvertedValue; 

if(Value1 ==0){

 BSP_LED_On(LED3);

}

else{

 BSP_LED_On(LED6);

}

 /* Infinite loop */

 while (1)

 {

 }

}

​

This topic has been closed for replies.

2 replies

oleksandr.karbivsky
Senior II
October 21, 2019

Hi. Try to put you led control code to ADC Conversion Comlete Callback.

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{ 
 uint32_t Value1 = 0;
 
 Value1=uhADCxConvertedValue; 
 
 if(Value1 ==0){
 BSP_LED_On(LED3);
 }
 else {
 BSP_LED_On(LED6);
 }
}

yuming
yumingAuthor
Associate
October 22, 2019

thank you oleksandr.karbivsky, I try to put to ADC Conversion Comlete Callback, and it's work now.